2016-11-10 6:10 AM
Good day!
I use microcontroller stm32l476ret.
In CubeMX create desired configuration and create project for Keil v.5.
The Keil everything compiles without errors.
Pour the code into the microcontroller.
The microcontroller runs and freezes on
ADC2 initialization error.If remove the ADC2 initialization code all working properly.
I tried to pass in debug mode -
see
that cycling is on ADC2 initialization error.I tried to do the minimum configuration: ADC2, SWD, quartz and GPIO.
Hangs on initialization.
Tried different modes ADC2 - the result of initialization error.
I am t
ried 2 different chips
This problem occurs only with the ADC2.
ADC1 and ADC3 working properly.
I am use CubeMX 4.17, fw package for stm32l4 1.5.2, Keil 5.21a.
Maybe it's a bug in the HAL?
2016-11-10 6:43 AM
Hello,
What about DMA configuration ?You can share your code to have more insight your ADC2 initialization and understand your issue.Regards2016-11-11 12:38 AM
Hello,
I am not use DMA. I am a little correct file stm32l4xx_hal_adc_ex.c and ADC2 was initialized OK. As I am see any peoples have problem with ADC2 initialization.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.