2016-02-13 2:22 AM
Hello!I have the follow problem:I use
STM32F745. I've chosen the
QuadSPI interface for flash, to be exact,
QSPI BANK2
. I make initialization through
CUBEMX, using HAL library. I see CLK signal only, there are no other signals. I've revised the generated code of initialization - it's ok. If I initialize
QSPI BANK1 - it's ok, there are all signals. I haven't met the definite prohibition of using
BANK2 separately.
CUBE lets initializing
BANK2 without using
BANK1. Now I'm working with
BANK2 due to initializing of regime of work with 2 flashes, and signals are duplicating.
The question is: is it possible to use
BANK2 separately? Where's the bug?
Any help appreciated!
#stm32f7-quadspi-bank22019-02-07 6:25 PM
Did this ever get resolved? I am also curious about using just Bank2.
2020-04-11 8:15 PM
hi, do you have solution now? thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.