2014-04-07 7:11 PM
Guys,
I have OV7670 module and STM32 dev board, I'm confused on how to connect the port of STM32 and OV7670 at the module because of the name of the port on OV7670 is different with in STM32 code, anyone has experience ? thanks
/*------------------------------------------------------
Ä£¿éÒý½ÅÃû³Æ | ÃèÊö | STM32¶ËÒý½Å�?¬½Ó |
------------------------------------------------------
SCCB_SCL : SCCBʱÖÓ : PB10 I2C2_SCL
SCCB_SDA : SCCBÊý¾�? : PB11 I2C2_SDA
CAM_VSYNC : Ö¡�?¬²½ : PA0 �?ⲿÖ�?¶�?0
CAM_HREF : FIFO : PB7 GPIO
CAM_WEN : FIFO�?´ÔÊ�?í : PD3 GPIO
XCLK : CMOS´«¸�?Æ÷Ö÷ʱÖÓ: PA8 MCOÊä³ö
CAM_RRST : FIFO¶�?µØÖ·¸´Î» : PE0 GPIO
CAM_REN : FIFOƬѡ : PD6 GPIO
CAM_RCLK : FIFO¶�?ʱÖÓ : PE1 GPIO
FIFO D0~D7 : FIFOÊý¾�?Êä³ö : PC0~PC7 GPIO
-----------------------------------------------------*/
2014-04-09 4:25 PM
On RCLK, what timing should I see ? I put like this
RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_4); //multiply by 4 = 32MHz and it's stable, but sometimes I can see it's late on scanning, still can see ''RGB'' on scanning....any ideas ? thanks2014-04-09 5:05 PM
On RCLK, what timing should I see ? I put like this
You should series of pulses as you bang it up and down in your loop.
FIFO_RCLK_H();
FIFO_RCLK_L();
2015-04-22 7:41 AM
Hello
I can write to registers but can't read them, what is the reason?I supply xclk pin with 42MHz sysclk coming from MCO2.Thanks.My problem was solved, it was related to the incompatibility of SCCB protocol andHAL_I2C_Mem_Read function of the stm32cubef4 software package.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.