STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SCCB and I2C problem

Posted on May 24, 2013 at 07:54Hi, I want to interface the OV7670 FIFO omnivision camera with STM32F4discovery board I have used an example inside of  STM32F4xx_DSP_StdPeriph_Lib_V1.1.0, the example drives an OV2640/9655 camera so I changed the regi...

girtor by Associate II
  • 2404 Views
  • 2 replies
  • 0 kudos

DCMI digital camera interface

Posted on November 20, 2013 at 15:14Hi everybody,I'm starting working with image sensors and there is something I don't understand.ST provides a digital camera interface called DCMI. I saw some people are using it OV7670 or OV5642. But in the sensor...

quentin by Associate
  • 1509 Views
  • 3 replies
  • 0 kudos

STM32f407 Discovery 10Mhz Clock Output?

Posted on March 06, 2014 at 10:42I want to use STM32F407 with the OV7670 camera. I need to external 10 MHz clock source.SystemCoreClock 168 MhzAHB Prescaler 1, ABP1 Prescaler 4, ABP2 Prescaler 2Can I get 10 Mhz clock using Timer 3. #stm32f407 #pw...

OV7670 interface cannot get product ID

Posted on July 11, 2012 at 00:52Hi,         I have a problem with interfacing OV7670 camera. I connect only 4 wires from Ov7670 to my stm32f4board, SIO_C, SIO_D, 3V+ and GND. Then I tried to read product id of the camera. It always send 0xFF. I am n...

theparitt by Associate II
  • 2735 Views
  • 6 replies
  • 0 kudos

STM32 port and OV7670 ?

Posted on April 08, 2014 at 04:11 Guys, I have OV7670 module and STM32 dev board, I'm confused on how to connect the port of STM32 and OV7670 at the module because of the name of the port on OV7670 is different with in STM32 code, ...

0690X00000602sPQAQ.jpg

ADC noise alternatives for 3-phase current measurement

Posted on April 17, 2015 at 12:48Hello again! I would like to make a question about an issue I have with the measurements of three currents! Specifically I have a 3-phase converter and I would like to measure its currents as fast and accurate as pos...

pant by Associate II
  • 2066 Views
  • 5 replies
  • 0 kudos

Overvoltage on GPIO pins (analog setup)

Posted on April 22, 2015 at 12:07I have a signal going into one of the pins on a STM32F303 which is set up in analog mode as an input to an ADC. It is fed by a 2K2 resistor. The power supply on the MCU is 3V. If the signal being fed into the 2K2 goe...

gbigden by Associate III
  • 1120 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.