2017-01-15 8:14 PM
Hi,
I am downloading an elf file to STM32 Nucleo-L053R8 board. The size of elf is given below:
text data bss dec hex filename
54700 728 3504 58932 e634 ../mDigitalIO_ADC.elfIn Linux, for the very first time, the elf successfully downloaded to the target and running properly. But next time if try to download I am facing the following issue:
No space left on device
If the board is disconnected and reconnected to the Linux machine the download is successful but the second time the same issue occurs.
But in windows, the repeated downloading to the target using simple copy commands works well and the elf runs successfully.
Is there any way to download the elf to Nucleo-L053R8 board without disconnect and reconnect on Linux machine without using st-link debugger instead using just 'cp' command.
Regards,
Raghavendra
2017-01-15 11:08 PM
Does you Nucleo board have a mbed bootloader (or similar) ?
This stuff usually emulates a mass storage device, where you just 'drop in' the executable. And in your case, that bootloader obviously wants to store a second executable 'file'. Not sure what goes on there.
But as a quick fix, you might try to remove the old version before ('rm' command), and pack it all into a script file.
2017-01-15 11:50 PM
You may need to flash the nucleo firmware.
https://developer.mbed.org/teams/ST/wiki/Nucleo-Firmware
https://developer.mbed.org/teams/ST/wiki/Nucleo-Firmware
I had a similar problem...
2017-01-15 11:59 PM
Is there any way to download the elf to Nucleo-L053R8 board without disconnect and reconnect on Linux machine without using st-link debugger instead using just 'cp' command.
You surely meant .bin rather than .elf
JW
2017-01-16 1:17 AM
Those convenience-bootloaders remind me too much of Arduino and similar 'stuff for superficials'.
First thing I always do is to remove them ...
2017-01-16 1:20 AM
Hi AvaTar,
Thanks for replying back.
The Nucleo board does have a similar mbed bootloader which is provided by ST and is called as ST-Link/v2-1. I updated the bootloader firmware of the device which is V2.J28.M18. Still the same issue.
'rm' command will not work because, as soon as executable is loaded the executable disappears.
Any other help is appreciated.
Regards,
Raghavendra
2017-01-16 3:20 AM
Hi,
I have updated the firmware with latest on Windows and using the board with Linux. After updating to latest firmware (V2.J28.M18) also, same issue continues.
Is it mandatory to update the firmware on Linux?
Regards,
Raghavendra
2017-01-16 3:21 AM
Yes, the executable is .bin which is derived from .elf.
2017-01-16 3:24 AM
I had update the firmware on two separate boards to resolve the need to disconnect and reconnect the USB cable..
it worked for Win10.
2017-01-16 4:47 AM
Hi
'No space left on device' ==> df -h
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.