STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G4 CRC DMA

Hello!So after few frustrating hours (as usually with ST), i reached the state when i found that CRC peripheral on STM32G4 (at least) DOES NOT SUPPORT DMA. Like are you kidding me? Is it for real? First of all i could not find a DMA request for CRC. ...

Eiffel by Senior
  • 2301 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 USB OTG Dual Role

HI team,          I am using STM32F7 series controller. I want to use USB OTG in dual mode where I want to run USB device and Host on same application. So till now I couldn't find a single application or sample related to this. Can anyone narrow down...

Shikamaru by Associate III
  • 8934 Views
  • 12 replies
  • 3 kudos

Uart Interrupt does not work

Hi, I am using the Nucleo - L152RE board and I am having a problem with the UART1 interrupt.The output to Teraterm works fine, but it does not go to the interrupt and the code terminates. Can you tell me what the problem is?  /* USER CODE BEGIN Heade...

Imhyeonu by Associate II
  • 2054 Views
  • 3 replies
  • 0 kudos

Resolved! Looking for a suitable MCU for USB to 4 UART and I2C

Hi Sir,I'd like to choose STM32F103V/R/Z to achieve the USB to 4UART and I2C in my system.Because it's said this MCU's USB support up to 8 bidrectional end ports. I don't know whether it's right or not.Could you help to review it or propose another s...

Bill_W_0-1724808371591.png
Bill_W by Associate II
  • 16811 Views
  • 13 replies
  • 12 kudos

Writing a program that updates itself at runtime

How can you write a program that updates itself for an STM32, eg. for an STM32F103C8?I'm not talking about a bootloader, since (as far as I know), a bootloader lives from (say) 0x08000000 to 0x08001000 in Flash and then updates another program (anoth...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.