2017-07-21 5:47 PM
I find when I make a call to HAL_I2C_Slave_Receive_IT it returns HAL_OK but it never manages to call the callback function, my HAL_I2C_SlaveRxCpltCallback(I2C_HandleTypeDef *I2cHandle) implementation.
Using a logic analyzer, I find that the device never acks the address and instead holds the clock line low till the device is reset.
I find if I use the synchronous api, HAL_I2C_Slave_Receive it ACKs and get's data just fine.
Also I am using the latest version of the STM32CubeMX + Keil ARM-MDK.
Any ideas? Thanks
Solved! Go to Solution.
2017-07-25 6:47 PM
So here is the result:
I2C1IRQ_handler --> HAL_I2C_EV_IRQHandler --> I2C_SLAVE_ISR_IT --> I2C_ITAddrCplt: which does nothing because the hi2c's state is 0x22 (HAL_I2C_STATE_BUSY_RX) instead of HAL_I2C_STATE_LISTEN.
I have external pull-ups on SDA and SCL.
Thanks.
2017-07-26 7:12 PM
I found that in I2C_ITSlaveCplt hi2c->XferCount is not 0 so it sets the error as HAL_I2C_ERROR_AF. The comments around the code says, 'All data are not transferred, so set error code accordingly'. I am not really sure what this means.
2017-07-26 7:58 PM
It seems like this code in stm32f0xx_hal_i2c.c is the culprit,
starting at line 4058:
/* All data are not transferred, so set error code accordingly */
if(hi2c->XferCount != 0U)
{
/* Set ErrorCode corresponding to a Non-Acknowledge */
hi2c->ErrorCode |= HAL_I2C_ERROR_AF;
}
I believe this check is not working as intended. If i remove it, everything works. It seems like there is an issue checking inequality between the two data types.
2017-07-27 5:29 AM
This means that not all information you tried to receive received!!
you put at HAL_I2C_Slave_Receive_IT(I2cHandle, (uint8_t *)aRxBuffer, RXBUFFERSIZE);
Means that RXBUFFERSIZE is bigger than the bytes you received , so adjust buffersize according the bytes you want to receive
A different aproximation is to wait for a fixed size 'header' which contains the length of a future transaction.
Also ,dont call transaction functions inside callbacks , you will face lock situations
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.