STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32f4 SPI data was broken

Posted on July 27, 2017 at 13:23Hi,I communicate with ADS1299(24bit, 8CH ADC chip) by SPI.ADS1299 SPI specification isCPOL=0 CPHA= 1Max SCLK = 20MHzand command flow is1) send read command(0x12)2) send dummy(x00) to make SCLK and receive 27 byte data...

0690X00000607dyQAA.png 0690X00000607e8QAA.png

Resolved! STM32 I2C HAL slave receive callback not called

Posted on July 22, 2017 at 02:47I find when I make a call to HAL_I2C_Slave_Receive_IT it returns HAL_OK but it never manages to call the callback function, my HAL_I2C_SlaveRxCpltCallback(I2C_HandleTypeDef *I2cHandle) implementation.Using a logic ana...

Arete sw by Associate II
  • 12614 Views
  • 13 replies
  • 2 kudos

How accurate is the internal RTC of STM32F407VG?

Posted on July 27, 2017 at 11:48I got to know that STM32F407VGT6 has an internal RTC support with either internal oscillator or an external one. Since the internal 32kHz oscillator is not that accurate, I would like to use an external 32kHZ oscillat...

SD_FindSCR Function Problem

Posted on July 27, 2017 at 10:56Hi,I use stm32f745 processor and SDMMC (SD 4 bits Wide bus ) at CubeMx. While sd card is writing data at every one minute, sometimes code is stopping at SD_FindSCR function in stm32f7xx_hal_sd.c library. This event is...

ali2399 by Associate II
  • 872 Views
  • 0 replies
  • 0 kudos

How to set LWIP debug to usart2 ?

Posted on July 24, 2017 at 10:29Hi,i already have done the setup for the lwip stack on the STM3210C-Eval board. I can already send via TCP/UDP and also RS232 to the uC (PC-->uC) and get also a echo back (uC-->PC). The debug output of the lwip-stack ...

HAL_CAN_Transmit timeout on STM32F429 using CubeF4 example

Posted on October 05, 2016 at 23:30 I'm having trouble implementing the STM32CubeF4 CAN example on my STM32F429I-Disco board. I'm using the CAN Network example provided with the STM324x9_Eval which in the readme.txt says: This example runs on STM32F...

16513584 by Associate II
  • 2569 Views
  • 5 replies
  • 0 kudos

Resolved! STM Flash Loader support for STM32F423 CPU missing

Posted on July 24, 2017 at 20:37Hello,The current version 2.8.0, and the pre-release version V2.9.0RC4 floating around in the forum, do not support the STM32F423 CPU. There is no map file for this CPU. Is there an updated pre-release of the program ...

STM32F303 Vih specification

Posted on July 26, 2017 at 03:40Data sheet for STM32F303 Vih specification indicates;1. TC and TTa I/O = 0.445*VDD + 0.3982.  FT and FTf  I/O =  0.5*VDD  + 0.23.  All I/Os except BOOT0 = 0.7*VDD.  Item 3 seems to contradict  1 and 2. Can this be cla...

D S by Associate
  • 1349 Views
  • 2 replies
  • 0 kudos

Resolved! RM0090: USART minimum attainable baudrate

Posted on June 29, 2017 at 17:15The mantissa in USART_BRR is 12-bit i.e. its maximum value is 4095. That limits accordingly the minimum attainable baudrate for given APB frequency.The following values in example tables are thus invalid and those bau...

0690X00000607WEQAY.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.