2019-08-13 3:11 AM
I am trying to use the built in boot-loader on my STM32F767. I wrote a simple app on my PC and I can get sensible answers from GET, GET VERSION, GET ID commands. But when I try to do a GO or a READ, the address (I have tries 0x00200000, 0x08000000 and 0 addresses) is rejected with a NAK.
Note that the READ or GO command itself is not rejected so it is not due to RDP or anything like that.
Any ideas why would be greatly appreciated.
So I got the STM Flash Loader Demo app to try that and it doesn't recognize my device.
If I try again I get a no response message unless I reset my board.
Any help on this would also be greatly appreciated.
Solved! Go to Solution.
2019-08-14 9:08 AM
Hello @KDuff.15 ,
The STM Flash Loader you are using does not support STM32F76x devices.
We recommend you to use the STM32CubeProgrammer software for programming STM32 products.
Best Regards
Imen
2019-08-13 3:16 AM
By the way, I am communicating using serial comms on USART1
2019-08-14 9:08 AM
Hello @KDuff.15 ,
The STM Flash Loader you are using does not support STM32F76x devices.
We recommend you to use the STM32CubeProgrammer software for programming STM32 products.
Best Regards
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.