2024-11-25 2:41 AM
Hello ST Community,
I’m working on a project where I initially developed software on the STM32H735 evaluation board. Now, I need to port this project to a custom board using the STM32H730 microcontroller. The external flash memory is the same as the one on the H735 (MX25LM51245GXDI00), with the only difference being three pins: DIO2, DIO4, and DIO6.
In my project, I use FATFS to load a .bin file into the external memory and then jump to execute it. I’ve also tested the external flash memory and confirmed that it works correctly on the custom STM32H730 board. This gives me confidence that the external memory is correctly wired and functional.
I’ve followed several tutorials, meticulously implementing all steps to create an external loader, including adding the required .c and .h files, linker scripts, and StorageInfo. However, I’m still stuck, and the loader does not work. Along the way, I’ve solved several compilation issues, such as:
One peculiar issue I’ve noticed is with the .stldr file. If I generate it using a Linux post-build command like:
arm-none-eabi-objcopy -O binary PlacaBoot.elf PlacaBoot.bin && cp PlacaBoot.bin PlacaBoot.stldr
The .stldr file is created (~200KB), but STM32CubeProgrammer does not recognize it.
On the other hand, if I rename the .elf file directly to .stldr (e.g., PlacaBoot.elf to PlacaBoot.stldr), CubeProgrammer recognizes it, but the file is around 2MB in size, significantly larger than the .stldr generated by the Linux command.
Could this size difference indicate an issue? I’ve also tried using:
cmd.exe /C copy /Y “${BuildArtifactFileBaseName}.elf” “${BuildArtifactFileBaseName}.stldr”
But since I’m on a Linux environment, the command fails because cmd.exe is not available.
Theoretically, if I modify the pin definitions in the external loader for the STM32H730 custom board to match the STM32H735G-DK board, the loader should work. However, I encounter the same issue on the STM32H735G-DK.
I’ve attached logs from STM32CubeProgrammer and my project files for review. I believe these might help pinpoint the issue. A working external loader project for the STM32H735 would also help as a reference, but it needs to be modifiable (not in .stldr format) so I can adjust the pin configuration.
I’ve been stuck on this issue for days now, and I would deeply appreciate any advice or guidance. If there’s any glaring mistake in my setup or approach that I might have missed, please let me know.
Thank you so much for your time and support!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.