2017-09-21 6:20 AM
I am using STM32F417IGH6 chip with ST-LINk V2, but ST-link is not detecting in the STM32 ST-Link utility software to program the ST. What all I should look into Hardware wise. I have checked the power, reset, everything looks fine. I am connecting the following signals in ST-LINK V2 to STM32
reset,
gnd
swdio
swclk.
2017-09-21 4:10 PM
External ST-LINK requires pin 1 to connect to your 3.0-3.3V supply (ie VTarget)
Chip orientation
Voltage on VDDA
Voltage on VCAP pins
State of NRST pin
Do you have a schematic? Everything being 'fine' doesn't get me closer to understanding what is 'wrong'...
Diagram trumps Prose
2017-09-22 5:16 AM
Hi, Thank you for the reply.
I checked the points mentioned by you. It is fine and while debugging, I found that, the SWDIO pin is LOW in non-working board and HIGH in working board when the board is powered ON. The board in which it is HIGH is connecting to ST LINK and where it is LOW, it is not connecting. Is this a problem? What is the default condition of SWDIO pin? Any other process to make this work? Please help.
2017-09-22 5:45 AM
Hello.
Take a look to this previous
similar like yours.2017-09-22 8:10 AM
>>
Any other process to make this work?
Saying some is 'fine' is unhelpful. Specifically what voltages do you see on the VCAP pins.
A device that is unpowered will be unresponsive. Focus on that, and the quality of your soldering, etc. Check for shorts/opens, check current consumption.
There isn't some wand waving exercise I can perform to make this work. If there are board manufacturing issues, or with components you will need to track those things down. As you have boards that work vs ones that don't focus on what differentiates them.
2017-09-22 8:24 AM
Hi,
I forgot to mention that, these boards were in working condition, before
we faced such issue.
Anyway I shall look into the things which you have mentioned.
2017-09-22 8:26 AM
https://community.st.com/0D70X000006SsWdSAK
If you have code that messes with the SWD pins or puts the device to sleep you can try pulling the BOOT0 High so it doesn't run your code, or try 'Connect under Reset' options.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.