2016-05-30 10:56 AM
Hello everyone,
I have some serious problems i want to send an array of data with SPI but that doesn't work i used the code from the snippet but i changed it a little bit but it doesn't work also in the code below you can see the code that i use , can someone help me please?#include ''stm32f091xc.h''
#include <stdio.h>
uint8_t SPI1_DATA[] = {0x00,0x00,0x00,0x00,0xE1,0xFF,0x10,0xFF,0xE1,0xFF,0x10,0x00,0xE1,0x00,0xFF,0x00,0xE1,0x00,0x00,0xFF,0xE1,0xFF,0xFF,0x00};
void
Configure_GPIO_SPI1(
void
);
void
Configure_SPI1(
void
);
int
main(
void
)
{
Configure_GPIO_SPI1();
Configure_SPI1();
while
(1)
{
if
((SPI1->SR & SPI_SR_TXE) == SPI_SR_TXE)
/* Test Tx empty */
{
SPI1->DR |= *SPI1_DATA;
/* Will inititiate 8-bit transmission if TXE */
}
}
}
__INLINE
void
Configure_GPIO_SPI1(
void
)
{
/* Enable the peripheral clock of GPIOA */
RCC->AHBENR |= RCC_AHBENR_GPIOAEN;
/* (1) Select AF mode (10) on PA4, PA5, PA6, PA7 */
/* (2) AF0 for SPI1 signals */
GPIOA->MODER = (GPIOA->MODER
& ~(GPIO_MODER_MODER4 | GPIO_MODER_MODER5 | \
GPIO_MODER_MODER6 | GPIO_MODER_MODER7))\
| (GPIO_MODER_MODER4_1 | GPIO_MODER_MODER5_1 |\
GPIO_MODER_MODER6_1 | GPIO_MODER_MODER7_1);
/* (1) */
GPIOA->AFR[0] = (GPIOA->AFR[0] & \
~(GPIO_AFRL_AFRL4 | GPIO_AFRL_AFRL5 |\
GPIO_AFRL_AFRL6 | GPIO_AFRL_AFRL7));
/* (2) */
}
__INLINE
void
Configure_SPI1(
void
)
{
/* Enable the peripheral clock SPI1 */
RCC->APB2ENR |= RCC_APB2ENR_SPI1EN;
/* Configure SPI1 in master */
/* (1) Master selection, BR: Fpclk/256 (due to C27 on the board, SPI_CLK is set to the minimum)
CPOL and CPHA at zero (rising first edge) */
/* (2) Slave select output enabled, RXNE IT, 8-bit Rx fifo */
/* (3) Enable SPI1 */
SPI1->CR1 = SPI_CR1_MSTR | SPI_CR1_BR;
/* (1) */
SPI1->CR2 = SPI_CR2_SSOE | SPI_CR2_RXNEIE | SPI_CR2_FRXTH | SPI_CR2_DS_2 | SPI_CR2_DS_1 | SPI_CR2_DS_0;
/* (2) */
SPI1->CR1 |= SPI_CR1_SPE;
/* (3) */
}
void
NMI_Handler(
void
)
{
}
void
HardFault_Handler(
void
)
{
while
(1)
{
}
}
void
SVC_Handler(
void
)
{
}
void
SysTick_Handler(
void
)
{
}
// Basis klokinstellingen doen
void
SystemClock_Config(
void
)
{
RCC->CR |= RCC_CR_HSITRIM_4;
// HSITRIM op 16 zetten, dit is standaard (ook na reset).
RCC->CR |= RCC_CR_HSION;
// Internal high speed oscillator enable (8MHz)
while
((RCC->CR & RCC_CR_HSIRDY) == 0);
// Wacht tot HSI zeker ingeschakeld is
RCC->CFGR &= ~RCC_CFGR_SW;
// System clock op HSI zetten (SWS is status geupdatet door hardware)
while
((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_HSI);
// Wachten to effectief HSI in actie is getreden
RCC->CR &= ~RCC_CR_PLLON;
// Eerst PLL uitschakelen
while
((RCC->CR & RCC_CR_PLLRDY) != 0);
// Wacht tot PLL zeker uitgeschakeld is
RCC->CFGR |= RCC_CFGR_PLLSRC_HSI_PREDIV;
// 01: HSI/PREDIV selected as PLL input clock
RCC->CFGR2 |= RCC_CFGR2_PREDIV_DIV2;
// prediv = /2 => 4MHz
RCC->CFGR |= RCC_CFGR_PLLMUL12;
// PLL multiplied by 12 => 48MHz
FLASH->ACR |= FLASH_ACR_LATENCY;
// meer dan 24 MHz, dus latency op 1 (p 67)
RCC->CR |= RCC_CR_PLLON;
// PLL inschakelen
while
((RCC->CR & RCC_CR_PLLRDY) == 0);
// Wacht tot PLL zeker ingeschakeld is
RCC->CFGR |= RCC_CFGR_SW_PLL;
// PLLCLK selecteren als SYSCLK (48MHz)
while
((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_PLL);
// Wait until the PLL is switched on
RCC->CFGR |= RCC_CFGR_HPRE_DIV1;
// SYSCLK niet meer delen, dus HCLK = 48MHz
RCC->CFGR |= RCC_CFGR_PPRE_DIV1;
// HCLK niet meer delen, dus PCLK = 48MHz
SystemCoreClockUpdate();
// Nieuwe waarde van de core frequentie opslaan in SystemCoreClock variabele
SysTick_Config(48000);
// Interrupt genereren. Zie core_cm0.h, om na ieder 1ms een interrupt
// te hebben op SysTick_Handler()
}
Greetz Sandeerius
#stm32f091 #spi
2016-05-30 12:50 PM
So use a pointer, and advance it?
uint8_t SPI1_DATA[] = {0x00,0x00,0x00,0x00,0xE1,0xFF,0x10,0xFF,0xE1,0xFF,0x10,0x00,0xE1,0x00,0xFF,0x00,0xE1,0x00,0x00,0xFF,0xE1,0xFF,0xFF,0x00};
void Configure_GPIO_SPI1(void);
void Configure_SPI1(void);
int main(void)
{
uint8_t *s;
int i;
Configure_GPIO_SPI1();
Configure_SPI1();
s = SPI1_DATA;
i = sizeof(SPI1_DATA);
while (i--)
{
if((SPI1->SR & SPI_SR_TXE) == SPI_SR_TXE) /* Test Tx empty */
{
SPI1->DR = *s++; /* Will inititiate 8-bit transmission if TXE */
}
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.