2023-06-05 6:00 AM
When I enable SPE for my Spi I receive 1 byte as expected, and the RXNE flag is set.
However, when I read the SPI1->DR value, it does not clear RXNE. I also noticed the OVR flag is set for some reason, even though I am reading the ->DR in the RXNE interrupt handler.
I'm sure I'm missing something simple :)
Solved! Go to Solution.
2023-06-05 6:39 AM
Which STM32?
> I receive 1 byte as expected
How exactly?
Note, that Rx-only mode clocks autonomously as long as SPE is enabled.
JW
2023-06-05 6:39 AM
Which STM32?
> I receive 1 byte as expected
How exactly?
Note, that Rx-only mode clocks autonomously as long as SPE is enabled.
JW
2023-06-07 10:14 AM
Thanks for the heads-up. I now see the clock continuously runs if SPE is enabled and in RXONLY mode. I ended up using FullDuplex and transmitting dummy bytes out for each byte received.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.