2023-06-05 12:23 AM
Hi,
I checked the default values of option bytes in STM32G071 by reading it from a device by using STM32CubeProgrammer.
I observed that values are not the same as it is specified in the RM0444.
I detected mismatch in value of PCROP1A_STRT registers and WRPxA_STRT registers.
I understand that this is related to the flash size. For example, the default value of the PCROP1A_STRT = 0x1FF (according the the RM0444), value actually written to MCU by ST is 0xFF.
In our test procedure it is specified that if PCB needs to be re-flashed, the option bytes are first cleared back to default and than the whole process of flashing and testing is repeated.
At this point, I do not know, what are the default values.
NOTE: on the MCU where I checked the default values of option bytes, they were not re-programmed yet.
Thank you for your response!
2023-06-05 1:39 AM
List of option bytes and their values read from MCU where they were not touched yet:
RDP=0xAA
BOR_EN=0x0
BORR_LEV=0x3
BORF_LEV=0x3
nRST_STOP=0x1
nRST_STDBY=0x1
nRST_SHDW=0x1
IWDG_SW=0x1
IWDG_STOP=0x1
IWDG_STDBY=0x1
WWDG_SW=0x1
RAM_PARITY_CHECK=0x1
nBOOT_SEL=0x1
nBOOT1=0x1
nBOOT0=0x1
NRST_MODE=0x3
IRHEN=0x1
PCROP1A_STRT=0xFF
PCROP1A_END=0x0
PCROP_RDP=0x0
PCROP1B_STRT=0xFF
PCROP1B_END=0x0
WRP1A_STRT=0x3F
WRP1A_END=0x0
WRP1B_STRT=0x3F
WRP1B_END=0x0
BOOT_LOCK=0x0
SEC_SIZE=0x0
2023-06-07 9:18 AM
Hello @Aljaž Krašna ,
There has been a case created to resolve this question and we will be reaching out to you directly.
Regards,
Roger
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.