2016-04-02 8:04 PM
To MCD Application Team and any professional,
I read through the source code of \STM32Cube_FW_F4_V1.10.0\Drivers\BSP\STM32F411E-Discovery\stm32f411e_discovery_audio.c as well as any stm32f4xx_audio.c file.I notice that in function BSP_AUDIO_OUT_Init(), the I2SCLK is set different for 2 different set of audio frequency, multiple of 8 (8k, 16k, 24k, 32k, etc.) and others (11.025k, 22.050k, 44.1k, etc)================Source Code============================
if((AudioFreq & 0x7) == 0)
{ /* Audio frequency multiple of 8 (8/16/32/48/96/192)*/ /* PLLI2S_VCO Output = PLLI2S_VCO Input * PLLI2SN = 192 Mhz */ /* I2SCLK = PLLI2S_VCO Output/PLLI2SR = 192/6 = 32 Mhz */ rccclkinit.PeriphClockSelection = RCC_PERIPHCLK_I2S; rccclkinit.PLLI2S.PLLI2SN = 192; rccclkinit.PLLI2S.PLLI2SR = 6; HAL_RCCEx_PeriphCLKConfig(&rccclkinit); }else
{ /* Other Frequency (11.025/22.500/44.100) */ /* PLLI2S_VCO Output = PLLI2S_VCO Input * PLLI2SN = 290 Mhz */ /* I2SCLK = PLLI2S_VCO Output/PLLI2SR = 290/2 = 145 Mhz */ rccclkinit.PeriphClockSelection = RCC_PERIPHCLK_I2S; rccclkinit.PLLI2S.PLLI2SN = 290; rccclkinit.PLLI2S.PLLI2SR = 2; HAL_RCCEx_PeriphCLKConfig(&rccclkinit); }================END=====================================What is the purpose for this setting??Thank you2016-04-03 5:38 AM
What is the purpose for this setting??
Presumably to allow you to hit the specific rates via the integer dividers used elsewhere?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.