STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

osxMotionFX libs and FreeRTOS

Posted on April 04, 2016 at 11:28Dear All,My colleagues and me are developing in very short time a new product with STM32 and STM MEMS.The hardware is on the go, and we are using Nucleo-L476-RG with X-NUCLEO-IKS01A1 and STEVAL-MKI160V1 for software ...

about timing using F446RE

Posted on April 03, 2016 at 04:39Hi all,   I got a board NUCLEO F446RE. I am using mbed for coding and I saw there are delay function precise up to microsecond. I need to create a series of TTL pulses with period in few microseconds to couple hundre...

llwaeva by Associate II
  • 3168 Views
  • 6 replies
  • 0 kudos

SPI clock is set different for different audio frequency

Posted on April 03, 2016 at 05:04To MCD Application Team and any professional, I read through the source code of  \STM32Cube_FW_F4_V1.10.0\Drivers\BSP\STM32F411E-Discovery\stm32f411e_discovery_audio.c as well as any stm32f4xx_audio.c file.I notice t...

simk0024 by Associate II
  • 1182 Views
  • 1 replies
  • 0 kudos

Problem while enabling I2C & FSMC in STM32F103ZE

Posted on June 29, 2015 at 12:06Hi,I am using STM32F103ZE microcontroller. In which  communicating with external SRAM with FSMC . It is working fine.1)Now I am trying to communicate with an IC which is connected through I2C1 (PB6 : SCL , PB7 : SDA,)...

grv1103 by Associate
  • 2735 Views
  • 5 replies
  • 0 kudos

STM32F429x.SVD

Posted on March 11, 2016 at 16:03I downloaded this from http://www.arm.com/products/processors/cortex-m/cortex-microcontroller-software-interface-standard.php and found what I think is an issue with FLASH.ACR.LATENCY: it’s described as 3 bits wide, ...

could not disable out protection

Posted on July 21, 2013 at 15:43hello every one.i have stm32f407 demo board that i cant program it any more. last program work correctly ,but if i want to erase the chip or program it again make the error stilinkv2/and st-link software error ''could...

ADC do not work in differential mode

Posted on March 26, 2016 at 07:54Good afternoon, I have problem in use ADC in differential mode. In differential ended mode  ADC do not work on my device and Nucleo-F334R8 also. I use Ac6 System Workbench, CubeMX and ST-Link V2 for develop. I do not...

STM32F7: stream video to micro SD

Posted on April 02, 2016 at 04:16What is the good way to store video capture from camera to microSD?I am using the lib ''sd_diskio.c''  to storage frame size 480x272x2 bytes but the quality is terrible, only 1 frame/second. It seems it took too much...

son1 by Associate II
  • 795 Views
  • 0 replies
  • 0 kudos

STM32F303K8 CAN Init failure on all modes

Posted on April 01, 2016 at 16:47 That's right, the very same acknowledgement error found during calls to CAN_init(CAN1, &CAN); is found waiting on the INACK bit to be cleared. And yes, the CAN clocks are turned on. This error is n...

troyerta by Associate II
  • 1820 Views
  • 3 replies
  • 0 kudos

Looking for a better EEPROM emulation for STM32F030

Posted on April 01, 2016 at 19:24I need to have a modest amount (say 512 bytes) of EEPROM emulation on my F030 design.  I found app note AN4061, but it only allows for swapping between two 1K pages of flash.Does anyone know of a better implementatio...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.