2022-08-26 1:57 AM
Dear Community,
i'm working on an 4 Slot SAI Interface with an STM32G4 Series MCU.
The FrameSync signal is kind of slow (~2kHz) so i want to use the Receive_IT() to throw an interrupt when 4 Slots (32Bit each) has received.
So after starting the ADC Hardware, i'm calling
HAL_SAI_Receive_IT(&hsai_BlockA1, (uint8_t*)sai_buf, 4);To start the SAI Receiver.
In the HAL_SAI_RxCpltCallback() Function, i'm currently just looking to the received data and then start the Receive_IT again (sai_buf is defined as extern in header):
void HAL_SAI_RxCpltCallback(SAI_HandleTypeDef *hsai)
{
uint32_t ch0_sample = sai_buf[0] & 0x00ffffff;
uint32_t ch1_sample = sai_buf[1] & 0x00ffffff;
uint32_t ch2_sample = sai_buf[2] & 0x00ffffff;
HAL_SAI_Receive_IT(hsai, (uint8_t*)sai_buf, 4);
}Now to the issue that i'm facing (for like 4h now without now clue what's wrong).
When placing a breakpoint in the Callback to check the Data, it works just fine and data seems to be valid. I can just click run and it stops immediately in the next Callback with new data.
However, when I remove the Breakpoint and click run, the
void HAL_SAI_ErrorCallback(SAI_HandleTypeDef *hsai)gets called immediately. When looking in the hsai handler, the SAI_DMA_ERROR code is set. That makes no sense to me since i'm not using the DMA in any way.
What am I missing here?
Thank you for your suggestions,
kind regards and have a good time!
Tony
EDIT: the sai_buf is defined as
uint32_t sai_buf[4];
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.