STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to free NUCLEO STM32 board pins for FMC interface use

I want to interface a Nucleo-H743ZI2 board (MB1364E) with a memory chip using STM32's FMC.In order to do this I need to free up the following 4 pins, to be used by the morpho connector:PE1, currently yellow user LED, needed for FMC_NBL1.PD8, currentl...

LFerr.8 by Associate II
  • 3453 Views
  • 5 replies
  • 0 kudos

Resolved! simple 3 Button Touch Key application using TSC on STM32L431 goes wrong when power supply drops from 3.3V to approx 3.0V then recovers to 3.3V.

simple 3 Button Touch Key application using TSC on STM32L431 goes wrong when VDD power supply drops from 3.3V to approx 3.0V (just above BOR level) then recovers to 3.3V.All 3 Buttons are read back as active from this point on. Has anybody experience...

SAI_DMA_ERROR while using Receive_IT()

Dear Community,i'm working on an 4 Slot SAI Interface with an STM32G4 Series MCU. The FrameSync signal is kind of slow (~2kHz) so i want to use the Receive_IT() to throw an interrupt when 4 Slots (32Bit each) has received. So after starting the ADC H...

TBaue.1 by Associate II
  • 1097 Views
  • 0 replies
  • 0 kudos

Resolved! stmpe811 I2C address on stm32f429i-disc1

I bought a stm32f429i-disc1 board and I want to learn how to communicate to stmpe811 with I2C protocol, now I'm a little confused. According to stmpe811's data sheet, its address is 0x82 because its A0 pin is connected to ground, but board's schemati...

0693W00000StmX5QAJ.jpg 0693W00000StmXPQAZ.jpg
许和平 by Associate II
  • 1976 Views
  • 2 replies
  • 0 kudos

STM32 - FMC and 16b SDRAM but 8b bus

Grettings,Can the FMC be configured to handle a similar configuration?I have an SDRAM that has byte enable pins to the upper and lower bytes (Disable -> High Z), but no pins available to map the 16 bits. So, at the moment I'm working with half the me...

0693W00000Stn4YQAR.png 0693W00000Stn5gQAB.png
Jda S.1 by Associate
  • 1076 Views
  • 1 replies
  • 0 kudos

HSI

Is there any information about long term stabiliy of the internal high speed oscillator (HSI)?

STM32F767/77 controller power consumption ?

I am exploring on controller selection. And need to know how much power is consumed by STM32F7 series controllers assuming that very few peripherals are used.It will have ADC, SPI, Timers, FLASH and FRAM access.So, wanted to know how much power it wi...

NM.1 by Associate II
  • 1495 Views
  • 1 replies
  • 0 kudos

Encoder mode counter division possibilities?

Now every rising and fall edge are counted which results in counter incrementing by 4. I see and have tried playing with Prescaler Division Ratio which should normally be the parameter to divide incremental number but it does not work on Encoder mode...

0693W00000Stgh4QAB.png
xgn by Associate II
  • 2006 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.