2015-05-28 10:17 PM
System Clock Configuration tool is doing a great job to generate init code for STM32F405RG however it does not support external clock oscillator which is fed into OSC_IN (pin 5) only. (meaning Osc not Crystal).
I suspect that the RCC_CR_HSEBYP bit setting does not support such hardware.Is there a code example for the required modifications into the tool generated system_stm32f4xx.c file ? #stm32f4-clock2015-05-28 10:51 PM
> Is there a code example for the required modifications into the tool generated system_stm32f4xx.c file ?
Maybe there is, but what prevents you from writing your own clock startup code? As you've remarked, the difference is only in setting one bit. JW2015-05-28 11:02 PM
Reassured this was tried. It still might be a hardware issue but I'm trying to ensure it's not a firmware one before running to the hardware guys ...
2015-05-28 11:14 PM
Hardware issue can be excluded by a single touch with a scope probe, 5 seconds of work plus half an hour to locate the oscilloscope if it does not sit on your desk... ;)
Which STM32 model exactly? Please post the content of relevant RCC registers. You try to run a simple blinkey to check, do you. JW2015-05-28 11:19 PM
Oh, and 5 more seconds to check CLK_OUT is floating, using a continuity tester (ohmeter, ''beeper''...) ;)
JW2015-05-29 10:56 AM
Don’t forget the half hour of tracking down the scope probe clips before giving up and using bit’s of wire.
Even if it does live on your desk.
2015-05-29 11:06 AM
:)
It's the power cord in our lab. If you find the scope, it never has a power cord. It appears to be a consumable disappearing at an alarming rate, regardless of how much we buy for spare. JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.