2026-03-16 3:00 AM
[PN]: EVSPIN32G4-DUAL
[VERSION]: MCSDK 6.3.2
[TOOL]: Firmware
[DETAILS]:
Hello,
I am working on a dual-motor application using the EVSPIN32G4-DUAL board with MCSDK 6.3.2.
I observe the following behavior:
when both motors are running at the same time, the speed regulation is stable
when only one motor is running, strong speed oscillations appear
This behavior is observed when running either motor alone. In other words, the issue does not seem to be linked to one specific motor channel.
The motors are custom motors designed/manufactured by us, with the following configuration:
5 pole pairs
Rs / Ls identified with the profiler
Hall phase shift = 121°
Rotor angle measured using Hall sensors
PWM frequency = 16 kHz
The attached speed plot illustrates the issue:
first phase: only one motor running → oscillations visible
middle phase: both motors running → stable behavior
last phase: only one motor running again → oscillations visible
The current regulator seems very stable, only the speed loop is going crazy when both motors are running.
So the surprising point is that the system is more stable when both motors are enabled than when only one motor is active.
[EXPECTED BEHAVIOR]:
I expect the speed regulation to remain stable both in:
single-motor operation
dual-motor operation
The target is to have similar speed control performance regardless of whether one motor or both motors are running.
[HOW TO REPRODUCE]:
Use EVSPIN32G4-DUAL with a project generated with MCSDK 6.3.2
Configure both motors with Hall sensors
Use the following motor parameters:
5 pole pairs
Rs / Ls identified with profiler
Hall phase shift = 121°
PWM = 16 kHz
Start only one motor and observe the measured speed
Speed oscillations appear
Then run both motors simultaneously
The measured speed becomes stable
Stop one motor again
The oscillations return on the remaining active motor
Thank you for your help.
Solved! Go to Solution.
2026-03-16 7:55 AM
Hello @IrianJ,
Using two Shinano motors and a Hall main speed sensor, the following speed behavior is observed:
Starting or stopping a motor does not affect the speed of the other motor.
At low speed, the Hall sensor average speed FIFO depth parameter in the Speed Sensing Config tab is reduced from 16 to 6. This adjustment may also help in your case.
Is there a mechanical or electrical link between your both motors?
2026-03-16 7:55 AM
Hello @IrianJ,
Using two Shinano motors and a Hall main speed sensor, the following speed behavior is observed:
Starting or stopping a motor does not affect the speed of the other motor.
At low speed, the Hall sensor average speed FIFO depth parameter in the Speed Sensing Config tab is reduced from 16 to 6. This adjustment may also help in your case.
Is there a mechanical or electrical link between your both motors?
2026-03-16 8:19 AM
Hello,
Thank you for your reply and for your suggestion.
On my side, I managed to get the motors working correctly in single-motor operation by drastically lowering the speed controller gains (Kp and Ki). After that change, the speed oscillations disappeared when only one motor was running.
This should not be an issue for our application, even with the reduced speed control bandwidth.
So this is an acceptable workaround for us, even if it does not really explain why this behavior was happening.
Regarding your question: there is no mechanical link between the two motors. The only link is electrical, because both motors share the same DC bus.
I will try to change the FIFO depth parameter but we can considered the topic closed as explained above.
Thank you again for your support.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.