STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F100: Problem with Stopmode

Posted on May 29, 2015 at 19:09Hi, I'm having problem with stopmode. I want to wake up uC with RTC Alarm in EXTI17.But when i use stopmode with statement PWR_EnterSTOPMode(PWR_Regulator_LowPower, PWR_STOPEntry_WFI), it didn't wait to RTC Alarm Event...

thanhnk by Associate
  • 1061 Views
  • 2 replies
  • 0 kudos

STM32F207ZE I2C fails during Master read

Posted on May 30, 2015 at 00:11 Hi, I'm using I2CSTM32F207ZET6. It usually works well, and we can usually read and write with no problems. However, there is a consistent error that pops up where, if we are reading a number of bytes sequen...

0690X00000605HQQAY.png

Running STM32F4 from an Oscilator

Posted on May 29, 2015 at 07:17System Clock Configuration tool is doing a great job to generate init code for STM32F405RG however it does not support external clock oscillator which is fed into OSC_IN (pin 5) only. (meaning Osc not Crystal).I suspec...

isaac by Associate II
  • 2638 Views
  • 6 replies
  • 0 kudos

How to manage stack access by Interrupts (STM32L100) ?

Posted on May 20, 2015 at 22:51Dear community,I want to send some data via UART directly to DMA without interruption. To solve this problem I use a custom FIFO stack from which the DMA feeds itself using its DMA interrupt-routine.The stack is filled...

jogerh by Associate II
  • 2462 Views
  • 6 replies
  • 0 kudos

Modifying Custom HID Application

Posted on October 05, 2013 at 22:03Hi;I am working on the Custom HID application which is in the St library and I use STM3210E-EVAL.  But this protocol transfer only 2 bytes (1 Byte Id + 1 Byte Data) so I modified the code and I transferred the 64 b...

prt by Associate
  • 1335 Views
  • 2 replies
  • 0 kudos

Trouble with USART_ReceiveData() and STM32F103 with Tera Term

Posted on May 29, 2015 at 17:20Hi,I would like assistance in determining why I cannot properly use the USART_ReceiveData() function with my SMT32F103RE. I have been using Tera Term with a SparkFun FT232R usb to serial breakout board. Printing to Ter...

leah by Associate
  • 1277 Views
  • 1 replies
  • 0 kudos

interrupt routine service latency in stm32f407

Posted on May 29, 2015 at 14:49HelloWhat is the delay between interrupt occurance(e.g. external interrupt on a pin) and interrupt service routine entry?by some initial measurements, it's about 30 cpu clocks.Is it interrupt type(external pin, specifi...

STM32Cube USB VCP on F401

Posted on May 29, 2015 at 12:36Hi,Having had a working USB VCP using the old non-cube drivers, I've spent the last week trying to get a reliable VCP with the new ones - and failing. In fact at one point just uncommenting some irrelevant and unused c...

gw by Associate II
  • 1121 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.