2026-04-16 6:44 PM - last edited on 2026-04-20 3:44 AM by mƎALLEm
Hello!
I am using a 32.768 kHz TCXO (TG-3541CE) as the LSE to count the RTC.
The MCU is an STM32L452RE.
At room temperature, the RTC operates correctly, but at high temperatures (around 50 °C), the RTC stops.
Strangely, once it has stopped, touching the MCU by finger causes the RTC to start running again.
Suspecting an issue with the TCXO, I tried a different TCXO, but the same behavior occurred.
When I added a 200 Ω damping resistor between the TCXO and the MCU, the RTC no longer stopped even when the temperature was raised to 60 °C.
This seems to have solved the problem for now, but I am concerned about whether 200 Ω is an appropriate value and whether this is truly a fundamental solution.
If you have any ideas about possible root causes or considerations, I would really appreciate your advice.
Solved! Go to Solution.
2026-05-07 1:04 AM
You may have replied to a spammer - these days they regurgitate the thread through AI to have them look legit, and try to inject a fradulent link. That post has been manually reviewed and removed.
As you use an external TCXO, LSE drive strength should be irrelevant (AI-generated text will mention it as a LLM is trained to infer that from "LSE problems".)
At this point there's probably not much the public forum here can do to help you. You may want to contact ST directly, through FAE or the web support form.
JW
2026-04-17 3:29 AM
Hello @Red_Mask and welcome to the ST community,
As you are using a crystal oscillator, try to isolate the crystal and supply it separately at 50°c, does it generate a normal output as for a room temperature? probe the output with an oscilloscope.
2026-04-17 4:58 AM
The RCC is set to LSE BYPASS ?
2026-04-19 7:07 PM
I have confirmed that the oscillator continues to output 32.768 Hz waveform even at temperatures above 50°C.
2026-04-19 7:08 PM
Yes. I have set the RCC to LSE BYPASS.
2026-04-20 3:39 AM
Can you reproduce the problem at a "known good" board such as Nucleo?
JW
2026-04-20 4:57 PM
OK! I will try it.
2026-04-26 7:39 PM
2026-04-27 2:57 AM
How are *all* the supply and ground pins of the mcu connected? Is the power supply rock stable?
Is it STM32L452RExx or STM32L452RExxP?
JW
2026-05-06 5:41 PM
The MCU is STM32L452RET6TR.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.