2026-04-27 11:03 PM
Hi,
I am working with a custom board using an STM32N657X0H3Q and cannot for the life of me bring about a reset via the NRST pin.
I have tried applying the workarounds from errata sheet ES0620 - Rev 3, sections 2.2.19 and 2.2.23, but my device still just hangs when any reset is attempted and needs a power cycle to recover.
In our setup:
Since it runs from AXISRAM1 which is where the errata recommends to place the First power-on reset flag, I instead decided to set the CORE_RESET_TYPE bit in the SYSCFG_CM55RSTCR register before each reset (in addition to resetting the clock switch control bitfields to their defaults).
Does this type of setup have any implications regarding using the SYSRESETREQ bit to generate a software reset?
Thank you
/ Silvia
Solved! Go to Solution.
2026-05-05 6:36 AM
Hi Romain
I managed to solve the problem! I went digging through the reference manual and found the RCC reset duration control register (RCC_RDCR). Setting the Minimum Reset Duration (MRD) bits makes the NRST pin reset work perfectly.
My sequence is now:
Thank you very much for your guidance
Best regards,
Silvia
2026-04-28 5:49 AM
Hello @silvia_b
If you apply workaround 2.2.19 from ES0620 Rev. 3 and if yout want to change the CORE_RESET_TYPE bit in the SYSCFG_CM55RSTCR register, you must enable the SYSCFG clock. This is mandatory for the proposed workaround.
Bit 0 – SYSCFGEN: SYSCFG enable bit in the RCC_APB4HENR register first.
/* Enable SYSCFG Clock */
__HAL_RCC_SYSCFG_CLK_ENABLE()
Then apply the workaround.
if (*init_p != 0x11223344) // First power-on reset is detected
{
*init_p = 0x11223344; // Change init_p variable to a known value
SYSCFG->CM55RSTCR |= 1; // Set power-on reset from NRST pin
__ISB(); // Instruction Synchronization Barrier
__DSB(); // Data Synchronization Barrier
NVIC_SystemReset(); // Generate a system reset
}
Note: This will added in the next ES0620 revision.
Best regards,
Romain,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-04-29 12:41 AM
Hello Romain,
Thank you for that info :)
Sadly, adding that call does not seem to help in my case. My device still just hangs.
Could my issue have something to do with this note from workaround 2.2.23?:
"To successfully switch from one clock signal to another, ensure that both clock signals are present at their clock
switch inputs before updating the control bitfield value to reflect the new clock switch state."
I wasn't quite sure how exactly to ensure this
/ Silvia
2026-04-29 1:21 AM
Hello @silvia_b
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-05-05 6:36 AM
Hi Romain
I managed to solve the problem! I went digging through the reference manual and found the RCC reset duration control register (RCC_RDCR). Setting the Minimum Reset Duration (MRD) bits makes the NRST pin reset work perfectly.
My sequence is now:
Thank you very much for your guidance
Best regards,
Silvia
2026-05-06 11:41 AM
Hello @silvia_b
Probably restoring the registers RCC_CCIPR6 through RCC_CCIPR13 to their default values is the key element.
That’s good news if you’ve fixed it.
Could you mark the answer as “Accept as Solution”?
Best regards,
Romain
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-05-07 1:10 AM
Hello Romain,
To be clear, I had tried applying the workarounds from sections 2.2.19 and 2.2.23 before starting this thread. A colleague of mine had also tried the same with no success.
I'm sure the workarounds (plus your tip about __HAL_RCC_SYSCFG_CLK_ENABLE) are essential for resetting to work, but it wasn't until I added the write to the RCC_RDCR register that I saw any success
Best regards,
Silvia
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.