2017-07-19 5:11 AM
Refering to page no 6 in mb1191.pdf which is available as STM32F746G-discovery Kit schematic.
The pin diagram of following two Arduino connector was incorrect, this need correction as follows:
1. CN4 connector has ARD_D5 pin mentioned as PA8 -> this is incorrect.
ARD_D5 pin should be connected with PI0 as per rest of schematic.
2. CN7 connector has ARD_D10 pin mentioned as PI0 -> this is incorrect.
ARD_D10 pin should be connected with PA8 as per rest of schematic.
Please! do this correction urgently. Otherwise it will create a lot of confusion regarding the hardware design.
2017-07-19 7:54 AM
Hello
GUPTA.NEERAJ
,Thank you for bringing this issue to our attention.
You are right,
I will highlight this typo error to correct it in coming releaseofSTM32F746G-DISCO schematics pack.
Best Regards
Imen
2017-07-19 12:02 PM
Reported two years ago...
https://community.st.com/0D50X00009XkgDCSAZ
https://community.st.com/0D70X000006SoTcSAK
https://community.st.com/0D50X00009XkZ5xSAF
2017-07-19 11:52 PM
Thanks for acknowledging this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.