2017-07-19 4:58 AM
I want to use ADC3_IN6 pin which alternate function of PF8 pin available on STM32F746G-discovery board in my project but when i refer to the table mentioned on page no 82 in datasheet available as en.DM00166116.pdf, It was found that AFx where x is number corresponding to alternate function of all ADC3 pins available was not written at all . Please! include AF number of ADCs in this document. This document needs correction urgently.
2017-07-19 6:17 AM
The ADC function of pins is not an Alternate Function.
You need to set the pin as Analog in GPIO_MODER to be connected to the ADC (and the Alternate Function table applies only when the pin is set to AF in GPIO_MODER).
JW
2017-07-19 6:42 AM
Hello,
ADC is not in Alternate Function !
ADC pins are mentioned in the pinout table as Additional functions and not
Alternate Function.
So, it's normal that are not in the Alternate Function table and there is no number.
Regards
Imen
2017-07-19 11:54 PM
Thanks for all of u who replied to my question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.