2017-07-19 9:26 PM
Hi ,
I ran into a lockup issue after FAULTMASK is set by cpsid f. The software is running in SDRAM, and MPU is enabled, so instruction can be executed from SDRAM. At last, I found the lockup issue is gone if HFNMIENA bit is set. But I don't fully understand why from the
STM32F7 Series Cortex�-M7 processor programming manual(PM0253):
HFNMIENA bit description:
Enables the operation of MPU during hard fault, NMI, and FAULTMASK
handlers. When the MPU is enabled: 0: MPU is disabled during hard fault, NMI, and FAULTMASK handlers, regardless of the value of the ENABLE bit. 1: The MPU is enabled during hard fault, NMI, and FAULTMASK handlers. When the MPU is disabled, if this bit is set to 1 the behavior is Unpredictable.Unless HFNMIENA is set to 1, the MPU is not enabled when the processor is executing the handler for an exception with priority �1 or �2. These priorities are only possible when handling a hard fault or NMI exception, or when FAULTMASK is enabled. Setting the HFNMIENA bit to 1 enables the MPU when operating with these two priorities.
From the description, does that mean
FAULTMASK is set will cause MPU is disabled if
HFNMIENA bit is cleared?
#mpu #faultmask #stm32f7We’re moving the ST Community to a new platform to give you a better and more reliable community experience.