2014-09-30 11:29 PM
Hi everyone,
I want to use my encoder with 32bit general purpose timer TIM2 on my STM32F429 Discovery board. I've connected pin PA0 ( TIM2_CH1) and pin PA1 ( TIM2_CH2) to my encoder, but it didn't work. The encoder count value returned only 0 and 1. Then I changed pin PA1 to PB3 ( TIM2_CH2), and it works normally. I've tested on my friend's STM32F4 Discovery board, it also works normally when I connected PA0 and PA1 to my encoder. But I don't know why it doesn't work with my board. Here's my code: void RCC_Config() { // Enable GPIO clock RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA|RCC_AHB1Periph_GPIOB,ENABLE); // Enable SYS clock //RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG,ENABLE); //Enable TIM RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2,ENABLE); } void GPIO_Config() { GPIO_InitTypeDef GPIO_InitStructure; //Encoder chanel GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOA, &GPIO_InitStructure); //Connect Timer Pins to AF Pins GPIO_PinAFConfig(GPIOA,GPIO_PinSource1,GPIO_AF_TIM2); GPIO_PinAFConfig(GPIOA,GPIO_PinSource0,GPIO_AF_TIM2); } void Encoder_Config() { TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_Period = 0xFFFFFFFF; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); TIM_ARRPreloadConfig(TIM2, ENABLE); TIM_SetAutoreload(TIM2,0xFFFFFFFF); //Debounce filter // TIM_ICInitStruct.TIM_Channel=TIM_Channel_1|TIM_Channel_2; // TIM_ICInitStruct.TIM_ICFilter=0x3; // TIM_ICInitStruct.TIM_ICSelection=TIM_ICSelection_DirectTI; // TIM_ICInit(TIM2, &TIM_ICInitStruct); // set them up as encoder inputs TIM_EncoderInterfaceConfig (TIM2, TIM_EncoderMode_TI12, TIM_ICPolarity_Rising, TIM_ICPolarity_Rising); // turn on the timer/counters TIM_ClearFlag(TIM2,TIM_FLAG_Update); TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); TIM_SetCounter(TIM2,0); TIM_Cmd (TIM2, ENABLE); } NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4); NVIC_Structure.NVIC_IRQChannel = TIM2_IRQn; NVIC_Structure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_Structure.NVIC_IRQChannelSubPriority = 0; NVIC_Structure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_Structure); } void TIM2_IRQHandler(void) { if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET) { if((TIM2->CR1)&0x10) // true = giam NumEncoder -= 0xFFFFFFFF; else NumEncoder += 0xFFFFFFFF; TIM_ClearITPendingBit(TIM2, TIM_IT_Update); } } Can anyone help me? I would appreciate any help in determining what my errors are. Thank you! And sorry for my bad English.2014-10-01 2:23 AM
Check SB2
2014-10-02 1:01 AM
Hi clive1,
Thanks for your answer but I think I've still not understood. SB2 on my board is currently being soldered. Do you mean that I have to use soldering iron to de-solder SB2?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.