STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

emulate EEPROM with STM32F407 flash memory

Posted on October 01, 2014 at 18:24Hi I use the routine listed below to read in flash area (sector 11) three words that contain values ​​of sampling and if the first value found is different, register the new three values. The problem is that the va...

gian0652 by Associate
  • 1325 Views
  • 2 replies
  • 0 kudos

PTP PPS output on stm32f407

Posted on September 30, 2014 at 17:07HelloI have a STM32F407ZGT6, silicon revision Z, and I'm trying to generate a 1PPS output (Pulse Per Second) on pin PG8, using the PTP. The PTP is working fine, correctly timestamping the PTP packets. In the refe...

renato1 by Associate II
  • 3504 Views
  • 5 replies
  • 0 kudos

STM32F415 read unprotect

Posted on October 02, 2014 at 08:03Hi there,I have a problem that I can't figure it out. I am coding an application that manages empty device through STM32 ROM BOOTLOADER. The problem is that when I send command for read unprotect, and check for it'...

matej2 by Associate II
  • 694 Views
  • 0 replies
  • 0 kudos

CAN TX Problem

Posted on October 01, 2014 at 19:44Hi ST Forum,Debugging a CAN TX message and can't really do it :(. I connected scope to PB13 and just see a high (3V) signal on the TX line. Anything wrong with my code below?I'm wondering if it's my CAN_mode. Can a...

I2C doesn't send data and...

Posted on September 26, 2014 at 15:16  The original post was too long to process during our migration. Please click on the attachment to read the original post.

flash timeout reset the target and try it again - error

Posted on July 25, 2013 at 14:52Hi All,I'm working on a STM32F0-Discovery kit. Until now, I could debug original code. I have succeed in loading the code which blinks an LED. I have even seen some minor modification's effect. I could have downloaded...

okerol by Associate
  • 4655 Views
  • 3 replies
  • 0 kudos

STM32F051K8 dies on setting PLLON

Posted on September 30, 2014 at 16:26 Dear community, I am having an issue with the setup of the PLL, which causes the CPU to jump into reset. Used libraries are libopencm3, toolchain is the latest arm-none-eabi release for linux (4.8 20...

p239955 by Associate II
  • 3004 Views
  • 7 replies
  • 0 kudos

STM32F030F4P6 - ADC 12b with DMA - 4 bits missing

Posted on October 01, 2014 at 17:04Hello Guys,I'm starting a new simple project with the STM32F030F4P6 chip and some analog sensors.In this project I need values from 3 channels from ADC1 (AN5:7) and send them to UART1. My problem is the value after...

maxime23 by Associate
  • 904 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.