2016-08-13 10:25 AM
Hi all! I'm trying to create a parallel synchronous data transmission using DMA and GPIO on a STM32F051 MCU. I've been following the AN4666 document that ST released, but is set up for STM32F4 MCUs. I also don't use HAL drivers, unlike the example code ST has for that document.
I'm having issues with getting the DMA to output data to the pins. I see only 0 on the pins. I should see all 1s as I set the data buffer to 0xFFFF for all location in the buffer. I'm guessing I don't have DMA set up properly or have it tied correctly up to TIM1. TIM1 is currently outputting a 20KHz PWM signal as expected.
#include ''base_lib.h''
/* Private typedef -----------------------------------------------------------*/
GPIO_InitTypeDef GPIO_InitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
DMA_InitTypeDef DMA_InitStructure;
static uint16_t asrc_buffer[FULL_FRAME_SIZE];
uint32_t counter=0;
/* Private function prototypes -----------------------------------------------*/
static void Data_GPIO_Config(void);
static void Timer_GPIO_Config(void);
static void ConfigureTIMxAsPWM_withDMA(void);
//static void SetupTimer(void);
/* Private functions ---------------------------------------------------------*/
/**
* @brief Main program
* @param None
* @retval None
*/
int main(void)
{
//Create data to be sent
for (counter = 0; counter <
FULL_FRAME_SIZE
- 1 ; counter++)
{
asrc_buffer[counter] &= 0xFFFF;
}
/* Configure the Data GPIO in output mode */
Data_GPIO_Config();
//Set up timer GPIO
Timer_GPIO_Config();
/* Start TIM PWM with DMA1 channel 5 */
ConfigureTIMxAsPWM_withDMA();
while (1){}
}
/**
* @brief Configure the Data GPIO in output mode
*
* @note None
* @param None
* @retval None
*/
void Data_GPIO_Config(void)
{
RCC->AHBENR |=RCC_AHBENR_GPIOCEN; // Enable GPIO port C
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOC, &GPIO_InitStructure);
}
/**
* @brief Configure the Timer GPIO
*
* @note None
* @param None
* @retval None
*/
void Timer_GPIO_Config(void)
{
RCC->AHBENR |=RCC_AHBENR_GPIOAEN; // Enable GPIO port A
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
//place before GPIO_Init to avoid pin being connected
GPIO_PinAFConfig(GPIOA,GPIO_PinSource9,GPIO_AF_2);
GPIO_Init(GPIOA, &GPIO_InitStructure);
}
void ConfigureTIMxAsPWM_withDMA(void)
{
/* TIM1 clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 , ENABLE);
/* DMA1 clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
uint16_t Period;
Period = 1000000 / 20000; // 20 KHz for 1MHz prescaled
/* Time Base configuration */
TIM_TimeBaseStructure.TIM_Prescaler = 48-1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStructure.TIM_Period = Period - 1;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
// Channel 2
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_Pulse = Period/2 ; //50%
TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low;
TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Reset;
TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCNIdleState_Reset;
TIM_OC2Init(TIM1, &TIM_OCInitStructure);
//reset DMA1 channel5 to default values
DMA_DeInit(DMA1_Channel5);
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&asrc_buffer; //Data source, aka our data buffer
DMA_InitStructure.DMA_DIR=DMA_DIR_PeripheralDST; // Memory to peripheral
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; //Always write to same register
DMA_InitStructure.DMA_PeripheralBaseAddr=(uint32_t)&(GPIOC->ODR); //Where we want to output the data
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; //Increment through data buffer
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; // 16-bit register
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; // 16-bit array
DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; //not circular
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_Init(DMA1_Channel5, &DMA_InitStructure);
// Enable DMA1 Channel5 Transfer Complete interrupt
DMA_ITConfig(DMA1_Channel5,DMA_IT_TC,ENABLE);
//Enable DMA1 channel IRQ Channel5 */
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel4_5_IRQn; //DMA1_Channel4 and Channel5 interrupts
NVIC_InitStructure.NVIC_IRQChannelPriority=0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
//Enable the TIM1 compare capture 1 dma requests
TIM_DMACmd(TIM1,TIM_DMA_CC1,ENABLE);
/* TIM1 Main Output Enable */
TIM_CtrlPWMOutputs(TIM1, ENABLE);
// turning on TIM1 and PWM outputs
TIM_Cmd(TIM1, ENABLE);
}
void DMA1_Channel5_IRQHandler(void)
{
//stop the clock cycles. TODO: use bare metal register instead
TIM_Cmd(TIM1,DISABLE);
if(DMA_GetITStatus(DMA1_IT_TC5))
{
//Clear DMA1 Channel5 Half Transfer, Transfer Complete and Global interrupt pending bits
DMA_ClearITPendingBit(DMA1_IT_GL5);
}
}
2016-08-13 12:14 PM
Use = 0xFFFF, not &= 0xFFFF, the array is probably already zero.
Check if DMA1 supports M2M operation, not sufficiently familiar with the F051, check RM2016-08-13 2:47 PM
Changed to =0xFFFF. From what the RM says, DMA1 should support M2M. My attempt is to go from memory-to-peripheral, which it also supports.
I did see in the RM on table 29 that for TIM1, I should be using Channel 3. It says for TIM1_CH2 the DMA request should be channel 3. I have changed that as well.2016-08-13 3:28 PM
Still not working, but I did find some potential help from an older forum post with a similar problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.