2017-08-03 12:44 AM
Hi everyone,
ì'm trying to use te OLED MCOT256064BA-WM with the SSD1322 Driver.
Is so frustrating to be in the situation that the code seems really correct at least , but the OLED don't still Work.
I need Help!
i'm using the STM32F412ZGTx, the OLED is a 256x64
The code is Here, i Think the problem is the initialization of the driver , at the Oscilloscope the SPI Communication seems ok !
Thank you very much for every incoming help!!
void Oled_setupSSD1233(void)
{ //Si esegue procedura di accensione riportata sul datasheet del SSD1322//1) Power on STM32 e quindi VCI,VDDIO (MCU 3,3v)
HAL_GPIO_WritePin(Oled_NSS_Port, Oled_NSS_Pin, 1); // trasmissione non attiva HAL_Delay(5); //5ms da datasheet bisogna aspettare almeno 1ms che la 3.3 V dal micro diventi stabile //2) Delay Minimum 1 ms HAL_GPIO_WritePin(Oled_RST_Port, Oled_RST_Pin, 1); //non attivo HAL_Delay(200); HAL_GPIO_WritePin(Oled_RST_Port, Oled_RST_Pin, 0); // Reset SSD1322// 3) // Display Off
//128MUX // column and address normals , Display start line is set at display ram address 0 // Normal scan direction COm Outputs // contrast control register set at 7FhHAL_Delay(50); //4) 100micros datasheet
HAL_GPIO_WritePin(Oled_RST_Port, Oled_RST_Pin, 1); // 5) Reset off HAL_Delay(200); //50m // HAL_GPIO_WritePin(OLED_PWR_EN_GPIO_Port, OLED_PWR_EN_Pin, 1); // 6) Power on Vcc (12V) da Switch HAL_Delay(500); //6) wait at least 200mS and than 300, Vcc become stableReset_Device(); //7) inizializzazione
HAL_Delay(300);
} void Reset_Device(void) { // Lots of reset/tweaking commands followdisplaySend(SEND_CMD, 0xFD); // Set Command Lock (MCU protection status) ok
displaySend(SEND_CMD, 0xAE); // Sleep On (DisplayOFF) ok, displaySend(SEND_DAT, 0x12); // = Reset Unlocked Oled driver , se Locked accetta solo il Comando FDhdisplaySend(SEND_CMD, 0xB3); // Set Front Clock Divider / Oscillator Frequency
displaySend(SEND_DAT, 0x91); // = reset / 1100b (0xD0) divide per due , selezionata frequenza che non so , boh!!!//displaySend(SEND_DAT, 0xC0); // frequenza oscillatore a quella di reset e divisore 0, PROVARE
//displaySend(SEND_DAT, 0xD0) prova anche questodisplaySend(SEND_CMD, 0xCA); // Set MUX Ratio
displaySend(SEND_DAT, 0x3F); // = 63dec = 64MUX da 0 a 63 , numero di Righe attive (settate) che verranno eseguite in un unico frame.displaySend(SEND_CMD, 0xA2); // Set Display Offset ok
displaySend(SEND_DAT, 0x00); // = RESETdisplaySend(SEND_CMD, 0xA1); // Set Display Start Line ok
displaySend(SEND_DAT, 0x00); // = register 00hdisplaySend(SEND_CMD, 0xA0); // Set Re-map and Dual COM Line mode
//displaySend2(SEND_DAT, 0x14,0x11); // = Reset except Enable Nibble Re-map, Scan from COM[N-1] to COM0, where N is the Multiplex ratio displaySend(SEND_DAT, 0x14); displaySend(SEND_DAT, 0x11);displaySend(SEND_CMD, 0xB5); // Set GPIO
displaySend(SEND_DAT, 0x00); // = GPIO0, GPIO1 = HiZ alta impedenza, Input Disabled //ok, ma capire cos'è!!!displaySend(SEND_CMD, 0xAB); // Function Selection
displaySend(SEND_DAT, 0x01); // = reset = Enable internal VDD regulator ok displaySend(SEND_CMD, 0xB4); // Display Enhancement A //displaySend2(SEND_DAT, 0xA0,0xFD); // = Enable external VSL (OK) displaySend(SEND_DAT, 0xA0); // = Low GS display quality, for Normal (reset) send 0xB5 //ok displaySend(SEND_DAT, 0xFD);displaySend(SEND_CMD, 0xC1); // Set Contrast Current //ok, ma capire cos'è
displaySend(SEND_DAT, 0x9F); // = reset (0x7F) // 0xffdisplaySend(SEND_CMD, 0xC7); // Master Contrast Current Control// ok
displaySend(SEND_DAT, 0x0F); // = no changedisplaySend(SEND_CMD, 0xB9); // Select Default Linear Gray Scale table//ok
displaySend(SEND_CMD, 0xB1); // Set Phase Length //ok displaySend(SEND_DAT, 0xE2); // = Phase 1 period (reset phase length) = 5 DCLKs, Phase 2 period (first pre- charge phase length) = 14 DCLKsdisplaySend(SEND_CMD, 0xD1); // Display Enhancement B //ok
//displaySend2(SEND_DAT, 0x82,0x20); // = Normal (reset) (0xA2) displaySend(SEND_DAT, 0x82); // n/a displaySend(SEND_DAT, 0x20);displaySend(SEND_CMD, 0xBB); // Set Pre-charge voltage
displaySend(SEND_DAT, 0x1F); // = 0.60 x VCC //okdisplaySend(SEND_CMD, 0xB6); // Set Second Precharge Period //ok
displaySend(SEND_DAT, 0x08); // = 8 dclks [reset]displaySend(SEND_CMD, 0xBE); // Set VCOMH
displaySend(SEND_DAT, 0x07); // = 0.86 x VCC //okdisplaySend(SEND_CMD, 0xA6); // Set Display Mode = Normal Display //ok
displaySend(SEND_CMD, 0xA9); // Exit Partial Display //ok
Clear_RAM(); // ClearDisplay(); //displaySend(SEND_CMD, 0xA4); // spegne solo tutti i pixels dello schermo , serve una funzione clear che setti anche le dimensioni dello schermo e abiliti la RAM displaySend(SEND_CMD, 0xAF); // Set Sleep mode OFF (Display ON) // HAL_Delay(10); //0.01s }void Clear_RAM(void){
unsigned char x,y;Set_Column_Address(0x00, 0x77); // ci sono 120 colonne comprendenti ognuna 4 SEG ( pixels) , 25674 = 64 (3Fh) (63 dec da 0 a 63)
Set_Row_Address(0x00,0x7F); // 128max, 63 dec , 0 a 63 sono 64 righe, dovrebbe essere impostata la dimensione dell'OLED 256x Set_Write_RAM(); for(y=0;y<128;y++){ for(x=0;x<120;x++) // 119 cicli
{ displaySend(SEND_DAT, 0x00); } } }void displaySend(uint8_t sendType, unsigned char v)
{ displaySendStart(sendType); // controlla sendType(comando o dato) e setta CD di conseguenza , attiva sempre CS displaySendData(v); // v trasmesso da SPI displaySendEnd(); //Chip Select alto }void displaySendData(unsigned char v)
{ //SPI.transfer(v); uint8_t aTxBuffer[] = {0x00}, aRxBuffer[] = {0x00}; aTxBuffer[0] = v; HAL_SPI_TransmitReceive(&OLEDspi2, (uint8_t *)aTxBuffer, (uint8_t *)aRxBuffer, 1, 250); }void displaySendStart(uint8_t sendType)
{HAL_GPIO_WritePin(Oled_NSS_Port, Oled_NSS_Pin, 0); // se non funziona OLED, Spostare in fondo alla funzione
if (sendType == SEND_DAT) { HAL_GPIO_WritePin(Oled_CD_Port, Oled_CD_Pin, 1); } else if (sendType == SEND_CMD) { HAL_GPIO_WritePin(Oled_CD_Port, Oled_CD_Pin, 0); }}
void displaySendEnd(void)
{ HAL_GPIO_WritePin(Oled_NSS_Port, Oled_NSS_Pin, 1); }void Oled_Loop(void)
{ displaySend(SEND_CMD, 0xA5); // Entire Display ON, all pixels turns ON in GS level 15 HAL_Delay(1000); } #oled #stm32-f Note: this post was migrated and contained many threaded conversations, some content may be missing.Solved! Go to Solution.
2017-09-12 1:36 AM
Problem Solved, the bug was a not clear specification of a FPC SMD Connector that i used on the board i've designed for the OLED !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.