2017-09-11 4:45 AM
Hi, I am using the STM32L152C- Discovery.
I am trying to run an example project from STM32CubeL1, however , I get the following error while running.
** Programming Started **
auto erase enabledInfo : Device: STM32L1xx (Cat.1 - Low/Medium Density)Info : STM32L flash size is 128kb, base address is 0x8000000STM32L152RCTx.cpu: target state: haltedtarget halted due to breakpoint, current mode: Thread xPSR: 0x61000000 pc: 0x2000000e msp: 0x20008000wrote 8192 bytes from file Debug/STM32L152C-Discovery.elf in 0.614524s (13.018 KiB/s)** Programming Finished **** Verify Started **STM32L152RCTx.cpu: target state: haltedtarget halted due to breakpoint, current mode: Thread xPSR: 0x61000000 pc: 0x2000002e msp: 0x20008000verified 4152 bytes in 0.061745s (65.668 KiB/s)** Verified OK **** Resetting Target **adapter speed: 240 kHzshutdown command invoked2017-09-11 5:59 AM
Hi
dev.dgoc
,1- Which
STM32CubeL1 versionare you using?
2- Which example did you looked to?
3-what is your IDE ?
Could you please provide more explanation on your case, so that it will be easier to understand the issue?
-Nesrine-
2017-09-11 7:29 AM
Hello!
In System Workbench for STM32 this is not an Error.
It means that the previous builded and linked image is succesfully loaded , verified and running.
Try to load the GPIO_IOToggle example for your discovery board to have visual evidence that the code is running.
Rgrds
vf
2017-09-11 11:48 PM
Thank you,
1- I am using STM32CubeL1_V1.7.0
2-I am trying to run GPIO_IOToggle example on AC6 (SW4STM32).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.