2017-12-11 8:06 PM
I'm trying to learn antenna matching and I'm as much a 'do the math' guy as I am 'hack it out through trial and error' kind of person. Usually it's both, when I'm not getting it. And I'm not getting tank circuits right and I dont have a large set of inductors to play with. Is there a chip that is a variable inductor with a digital interface? I should have just built the oatmeal container radio and moved on to motor controls.
:)
2017-12-14 2:15 AM
RF circuits are usually electronically tuned with varactors, capacitors that vary in value with DC bias. You could achieve a similar effect with saturable inductors where you use a DC bias winding to adjust the core permeativity using the non-linear behaviour near saturation. Having said that, I doubt it's easy at RF frequencies.
I also think you really are going to be better off with a pre-approved module (including antenna) as the cost of certifying your own module will probably be $50,000 to $100,000.
2017-12-14 3:42 AM
using the non-linear behaviour near saturation. Having said that, I doubt it's easy at RF frequencies.
Huh, easy or not, I wouldn't want to do that in RF, generating a slew of harmonics. which in turn need then to be suppressed somehow....
JW
2017-12-15 2:31 AM
I offer it more out of academic interest than as a practical suggestion
2017-12-15 3:01 AM
Varactors would be less academical, with tuning achieved by driving the bias voltage with the DAC.
Just some level-shifting circuitry is required.
However, I do not see a convincing reason for a standard MCU in this context - the IF frequencies are a bit over the head to process, and the audio can be done much cheaper.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.