STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

how dose function name connect to interrupt address

Posted on December 13, 2017 at 13:20hi.i am writing a code for Exti interrupt  and i do that. But i get a qustion .when we want to use interrupt , I mean when the interrupt happen , then cpu jump to that interrupt address and the function that we wr...

two can bus with stm32f407 at the same time

Posted on December 15, 2017 at 11:32hi i want to have two can bus with stm32f407 can1 and can2. can1 for node 1 to 5 and can2 for node 6 to 10. but i receive data just in one bus at the same time. how should i config can1 & 2 in this case?

I2C on STM32F4, missing TX after sending Address, Data

Posted on December 14, 2017 at 22:21Hi,I'm using a STM32F429l-DISC1 Board and trying to get I2C working.Somehow my code fails, and I come back to the code from:https://sites.google.com/site/johnkneenmicrocontrollers/18b-i2c/i2c_stm32f407Now I want t...

uli stone by Associate II
  • 1292 Views
  • 1 replies
  • 0 kudos

why STM32f103C8 doesn't have Alarm option in CubeMX?

Posted on December 11, 2017 at 17:13Hello,In STM32F103C8 it states that it's possible to have Alarm set and use the interrupts , however in CubeMX there's no option for generating the code like the Other MCU which have Calender as well.Page 491 of  ...

0690X00000609ATQAY.png

Resolved! I cant download reference manual for stm32H7

Posted on December 14, 2017 at 14:00I cant download reference manual for stm32H7. https://community.st.com/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Freference_manual%2Fgroup0%2Fc9%2Fa3%2F76%2F...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.