2025-03-04 9:08 PM
I am using STM32s NUCLEO-H755ZIQ board , while debugging through eclipse IDE for the M7 core the board's MCU went under low power state and LD6 which is over current led (red) is turned on.
When I am connecting the board with the STM32CubeProgrammer the board is gettting detected but ST-Link is failing to flash the board.
Please help me with this problem as same thing has happend with the another NUCLEO-H755ZIQ board.
Both the boards are having same problem
Solved! Go to Solution.
2025-03-05 2:46 AM - edited 2025-03-05 3:01 AM
In that case either:
1- This regulator is internally short-circuited :
2 - Or you have a short circuit on the board.
To differentiate between the two cases you need to unsolder SB2 and fit again JP2.
If LD6 is lit: the regulator is broken. You need to purchase another board.
If LD6 is off you have a short circuit on the board. In that case you need to check your board and find if VDD is short-circuited.
Hope that helps.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.