2025-02-25 8:10 AM
Hi @guru ,
In Nucleo-G474RE ,I have connected W25Q16JV in quadSPI bank1 .I have written the Application image binary(.bin) in external flash.I am able to verify the binary written at 0x90000000it in memory mapped mode.When I do Jump to application to external flash from my code in internal flash.
SysTick->CTRL = 0;
// Set the stack pointer_
__set_MSP(*(__IO uint32_t*)APP_START_ADDRESS);
// Get the application entry point
void (*app_entry)(void) = (void (*)(void))(*(__IO uint32_t*)(APP_START_ADDRESS + 4));
// Jump to the application
app_entry();APP_START_ADDRESS given as 0x90000000.On jumping to application ,it doesn't execute.
When verified the example STM32G474E-EVAL,in that,for execute-in-place a fuction is written in external flash and called from internal flash.But I need to do jump to a application flashed in external flash.Any help on this ,would be highly appreciable.
Thanks,
Radhai
2025-02-25 7:41 PM
Hi,
Could someone advise on the above issue.
Thanks,
Radhai.E
2025-02-25 7:46 PM
> On jumping to application ,it doesn't execute.
What does it do? Does the PC register get updated? Debug, step through, see what the processor is doing.
There is example jump to bootloader you can use as a resource, except substitute the external flash address.
2025-02-25 9:36 PM
Hi,
Thanks for your reply,Could you please provide the link to the example you are mentioning.And ,a basic question ,does stm32G474RETX support jump to application in external flash from bootloader code in internal flash?.Any example would be highly helpful.
Thanks and regards,
Radhai.E
2025-02-26 6:53 AM
How to jump to system bootloader from application ... - STMicroelectronics Community
2025-03-05 3:12 AM
Hi @TDK ,
Thanks for your reply,Figured out my mistake I
I have added QSPI (rx) : ORIGIN = 0x90000000, LENGTH = 1024K in linker memory definition and issue got resolved.Now able to execute applicaiton in external flash
Thanks and regards,
Radhai.E
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.