2020-09-12 1:02 AM
Hello,
I am trying to read single ADC channel using NUCLEO-H743ZI2 board but the result is wrong. I have created a very simple project using CubeMX. Kept the default Clock setting. Enabled ADC3 CH0 (PC3_C Pint) in single ended mode polling. Enabled UART3 to print the message using on board VCP. But the adc return value is not correct. When i connect PC3 Pin to GND, value is around 4650-4750. I have tried many other combinations, but could not figure out what wrong i did. Can someone help me to solve ADC reading error. Initialization code is as bellow.
ADC Value Read :
uint16_t ADC_Raw;
while (1)
{
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
HAL_ADC_Start (&hadc3);
HAL_ADC_PollForConversion (&hadc3, 100);
ADC_Raw = HAL_ADC_GetValue (&hadc3);
My_Printf("\r\n CH%d[%d] ",0,ADC_Raw);
HAL_ADC_Stop(&hadc3);
HAL_Delay(1000);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
System Clock Configuration :
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Macro to configure the PLL clock source
*/
__HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSI);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USART3|RCC_PERIPHCLK_ADC;
PeriphClkInitStruct.PLL2.PLL2M = 32;
PeriphClkInitStruct.PLL2.PLL2N = 129;
PeriphClkInitStruct.PLL2.PLL2P = 2;
PeriphClkInitStruct.PLL2.PLL2Q = 2;
PeriphClkInitStruct.PLL2.PLL2R = 2;
PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_1;
PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOWIDE;
PeriphClkInitStruct.PLL2.PLL2FRACN = 0;
PeriphClkInitStruct.Usart234578ClockSelection = RCC_USART234578CLKSOURCE_D2PCLK1;
PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL2;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
ADC Configuration :
static void MX_ADC3_Init(void)
{
/* USER CODE BEGIN ADC3_Init 0 */
/* USER CODE END ADC3_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC3_Init 1 */
/* USER CODE END ADC3_Init 1 */
/** Common config
*/
hadc3.Instance = ADC3;
hadc3.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV256;
hadc3.Init.Resolution = ADC_RESOLUTION_16B;
hadc3.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc3.Init.LowPowerAutoWait = DISABLE;
hadc3.Init.ContinuousConvMode = DISABLE;
hadc3.Init.NbrOfConversion = 1;
hadc3.Init.DiscontinuousConvMode = DISABLE;
hadc3.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
hadc3.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
hadc3.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc3) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_64CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
sConfig.OffsetSignedSaturation = DISABLE;
if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC3_Init 2 */
/* USER CODE END ADC3_Init 2 */
}
Regards,
Asish Banerjee
Solved! Go to Solution.
2020-09-20 7:40 AM
Dear All,
My problem solved. It was the resistance of ground wire which was causes problem. It took a bit long time to short out the problem as we was first time using STM32H7 MCU. Thanks TDK for your support.
Regards,
Asish Banerjee
2020-09-12 4:26 AM
Hello,
Can anyone help me in this issue? I got stuck as i am working on a project where i have to use 16 bit ADC. That is why i am trying with STM32H743ZI MCU and need to work fast for the prototype.
Regards,
Asish Banerjee
2020-09-12 5:17 AM
> Enabled ADC3 CH0 (PC3_C Pint)
ADC3_CH0 is on PC2, not PC3.
2020-09-12 5:21 AM
Thanks TDK for your reply. Actually it is PC2 pin which i have used. By mistake i have mentioned PC3 here. Problem has not been shorted out yet. Is any other settings required to make it up?
Regards,
Asish Banerjee
2020-09-13 11:16 PM
Can anyone share NUCLEO-H743ZI2 ADC working sample project for STM32CubeIDE?
Regards,
Asish Banerjee
2020-09-14 6:27 AM
2020-09-14 8:17 AM
Dear TDK,
Thanks for the link. I have tried with that code also and result is if i connect PA6 pin to GND, adc value is around 1400-16000 and if i connect PA6 pin to 3.3V, adc value is around 30000-33000.
Regards,
Asish Banerjee
2020-09-20 7:40 AM
Dear All,
My problem solved. It was the resistance of ground wire which was causes problem. It took a bit long time to short out the problem as we was first time using STM32H7 MCU. Thanks TDK for your support.
Regards,
Asish Banerjee
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.