STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unstable Current Consumption in Low Power Mode

Greetings From Turkey, We have a hardware using stm32l471. We wake up at certain times and send data to the server. Then we go back to sleep mode.Here is the our callback to switch to low power consumption mode.void low_power_callback (int time) { s...

VÜnal.1 by Associate II
  • 1786 Views
  • 2 replies
  • 0 kudos

Resolved! Preserve a section of FLASH memory during programming

Following in the directions of this post, I am able to reserve and write to (and read back) from a section of FLASH dedicated to calibration data. However, when I reprogram the device, the IDE wipes the whole memory clean before programming and we lo...

JMill.1 by Associate III
  • 5049 Views
  • 3 replies
  • 0 kudos

Resolved! NUCLEO-H743ZI2 ADC Polling gives wrong result.

Hello,I am trying to read single ADC channel using NUCLEO-H743ZI2 board but the result is wrong. I have created a very simple project using CubeMX. Kept the default Clock setting. Enabled ADC3 CH0 (PC3_C Pint) in single ended mode polling. Enabled UA...

ABane.1 by Associate III
  • 3410 Views
  • 7 replies
  • 0 kudos

Resolved! STM32H750 ignores pull-up resistor when EXTI is selected

On F1xx and F4xx platforms, I have been using the GPIO pull-up resistors for the connections to OC hall sensors used in BLDC motors. There has never been a problem. With STM32H750, I can see that the PUPDR register has the right values for the pull...

olavi by Associate III
  • 2882 Views
  • 7 replies
  • 0 kudos

Resolved! What is "LSE drive"?

I'm trying to figure out the battery consumption of an STM32F746. Accodring to the datasheet, that depends on SRAM state, RCC state, and if the LSE is in low, medium low, medium high, or high drive.I have no idea what these kinds of drives are, nor ...

Dear Ladies and Gentleman I'm a student of the University HSLU. At the moment I have been working on an porject in which I have to implement a controllsystem that is controlling and measuring the temperature and values in a bio reactor.

The bio reactor has bone marrow inside of it and this is being analysed for the properties of microgravitation.I would use a NUCLEO-F303K8 microcontroller. The system must endure a maximum accelaration of 10G due to the fact that it will be used late...

HMate.1 by Associate
  • 893 Views
  • 1 replies
  • 0 kudos

Strange values from HAL_TIM_ReadCapturedValue

I'm using input capture with a 16 bit timer to read a 1.5ms pulse that occurs every 20ms. I can see on my scope that the input pulse conforms to this exactly. Here's the code for the interrupt callback:uint16_t pwmVal0 = 0; uint16_t pwmVal1 = 0; ...

0693W000004GTTAQA4.png
iforce2d by Associate III
  • 3785 Views
  • 5 replies
  • 0 kudos

USART Idle Interrupt without RXNE

I am working with the STM32F767 and DMA1/USART3 for RX and TX. TX is fully functional. Currently the idle line interrupt continuously fires when enabled, while the RXNE interrupt never fires. The Idle interrupt is cleared everytime the interrupt is f...

EBepp by Associate II
  • 3133 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.