2018-09-04 7:57 AM
Hello ST Community,
I am currently working on a prototype using a SPBTLE-RF module for Bluetooth communications. The module is connected with a SPI bus to a STM32L476VGT6 MCU to control it.
The problem is, I didn't find anything in the documentation about piloting the SPBTLE-RF with a MCU trough a SPI bus. (i didn't even found the commands)
So i am asking if you have any documentations with the method and the commands to use the SPBTLE-RF as a standalone.
Best regards,
Mickaël Aliot.
2018-09-11 1:50 AM
A little update, i found X-CUBE-BLE1 with code exemple, but i don't find how to use the bluetooth in an other way than in the example. The code is too complexe to read.
I only need to take data from my MCU and send it with the bluetooth (configured as host) to an other device.
2019-01-18 4:29 AM
Hello,
I was searching the same thing. Did you find any thing?
Best regards
Maxime
2019-03-08 4:17 AM
Hello,
Try this one - UM1865.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.