STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CubeMX 4.24 generates uncompilable code for TrueStudio

Posted on January 31, 2018 at 11:17Hello everyone,after update of STM32CubeMX it started to generate simply uncompilable code for TrueSTUDIO.When I select FATFS od FREERTOS and TrueSTUDIO as a IDE, after compilation,functions like HAL_Init(), osThre...

STM32H750 - Which is pin 1 corner ?

About to put my first device in the programmer and don't want to make a mistake. Datasheet says there is a round mark in the corner near pin 1, but of course the package has two round marks on diametrically opposite corners. With the writing correc...

MikeDB by Lead
  • 1651 Views
  • 2 replies
  • 0 kudos

Nucleo board G071RB$AU1

Hello,I just got an STM32G071 board - NUCELO-G071RB with an unusual label "NUG071RB$AU1".Is it some kind of preproduction sample?Thank you,David

F4 RTC prescalers computation

Hello,On STM32F429, I'm using RTC. It is clocked by the 32KHz LSI.I set async prescaler register to 127 and Sync prescaler register to 249.The total prescaling factor will be 250*128 = 32 000.Exactly what I need to provide 1Hz to RTC.After testing, i...

JulienD by Senior
  • 1902 Views
  • 5 replies
  • 0 kudos

Resolved! IAR "download and debug" reset registers ?

Hello,I am using a Bootloader which jump to operational application.the Bootloader configures SRAM, so that operational does not need to do it again.Bootloader is baremetal , and operational is freeRTOS.I use IAR.Everything works well if I reset the ...

ranran by Senior II
  • 1197 Views
  • 1 replies
  • 0 kudos

CAN working on STM32F446RET6U but not on STM32F446RET6

I made several custom PCBs using the STM32F446RET6 chip. At first the CAN seemed to work fine, by reading it out with a Kvaser (CAN sniffer). However problems arrived when attaching other devices (like a beagle bone) to the CANbus. The beagle bone on...

0690X0000087dEmQAI.jpg 0690X0000087dEcQAI.jpg 0690X0000087dEXQAY.jpg
MScho.4 by Associate
  • 991 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.