2024-06-09 6:05 AM
Hello Friends
I load mdk540.exe to my computer 5 times. But gives me an error like below.
I could not resolve this. anybody can help me as soon as possible please.
Many many thanks for nice and kind helping.
Sincerely
".../AppData/Local/Arm/Packs/Keil/STM32F1xx_DFP/2.4.1/Device/StdPeriph_Driver/src/misc.c(131): error: no member named 'IP' in 'NVIC_Type'
131 | NVIC->IP[NVIC_InitStruct->NVIC_IRQChannel] = tmppriority;"
2024-06-09 6:57 AM
Five times? Probably not an installation problem then..
More likely that you're trying to use the SPL (Standard Peripheral Library) and not the current HAL/Cube libraries.
What specifically are you trying to build?
Unpack the CubeF1 .ZIP file and descend into the example projects, and MDKARM project files
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.