2017-06-12 9:53 AM
hi everybody
i have a assembly program and want to use it in my project . but keil don't compile this directly. i don't have enough knowledge to correct and convert code to keil could compile this code. pls help me microcontroller in my project is stm32f4 family tnx alot.syntax unified
#ifdef __ARM_PCS_VFP
@ High-throughput block transfer using the FPU register set as a 128-byte
@ buffer.
@
@ This implementation exploits the IT Folding feature of the Cortex-M4.
@ An IT instruction following a 16-bit Thumb instruction, when both are
@ aligned into a 32-bit memory word, takes no additional cycles to issue.
@
@ Arguments:
@ r0 source address
@ r1 destination address
@ r2 number of words to transfer.
.section .ramcode,'ax',%progbits
.balign 4
.global _Z10copy_wordsPKmPmm
.thumb_func
_Z10copy_wordsPKmPmm:
@ Name our registers.
src .req r0
dst .req r1
count .req r2
@ The caller may have been using floating point.
@ Save the callee-save portion of the register file.
vpush {s16 - s31} @ 17
@ 'Warm up' the transfer engine, which wants to operate in units of
@ 128 bytes, by making smaller transfers until count a multiple of
@ Special-case the single word transfer; the macro below won't work.
lsrs.n count, #1 @ 1
itt cs @ 0 (aligned)
vldmcs.32 src!, {s0} @ 2
vstmcs.32 dst!, {s0} @ 2
@ Transfer n+1 words.
.macro XFER n @ 5 + 2*n
lsrs.n count, #1 @ 1
itt cs @ 0 (aligned)
vldmcs.32 src!, {s0 - s\n} @ 1+1+n
vstmcs.32 dst!, {s0 - s\n} @ 1+1+n
.endm
XFER 1 @ 7
XFER 3 @ 11
XFER 7 @ 19
XFER 15 @ 35
@ Handle the case where we've been asked to transfer <32 words.
@ In such a case, count will now be zero, and the Z flag will still
@ be set from the last XFER.
@
@ Force the branch to use a 32-bit instruction to preserve alignment
@ of the loop branch below; this saves a cycle per time that branch
@ is taken.
@
@ Note that the target of this branch (at 1 below) is also aligned,
@ saving a cycle on the rare escape path.
beq.w 1f @ 1 (n.t.)
@ All warmed up, transfer in units of 128 bytes.
0: vldm.32 src!, {s0 - s31} @ 33
vstm.32 dst!, {s0 - s31} @ 33
subs.n count, #1 @ 1
bne.n 0b @ ~3 (taken)
@ Restore FPU state.
1: vpop {s16 - s31} @ 17
bx lr @ 1-3??
#else
#error copy_words is not available for your architecture.
#endif�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
2017-06-12 8:11 PM
; .s built using FPU support, ie --cpu Cortex-M4.fp
; High-throughput block transfer using the FPU register set as a 128-byte
; buffer.
;
; This implementation exploits the IT Folding feature of the Cortex-M4.
; An IT instruction following a 16-bit Thumb instruction, when both are
; aligned into a 32-bit memory word, takes no additional cycles to issue.
;
; Arguments:
; r0 source address
; r1 destination address
; r2 number of words to transfer.
_Z10copy_wordsPKmPmm PROC
EXPORT _Z10copy_wordsPKmPmm
; The caller may have been using floating point.
; Save the callee-save portion of the register file.
vpush {s16 - s31} ; 17
; 'Warm up' the transfer engine, which wants to operate in units of
; 128 bytes, by making smaller transfers until count a multiple of
lsrs.n r2, #1 ; 1
itt cs ; 0 (aligned)
vldmcs.32 r0!, {s0} ; 2
vstmcs.32 r1!, {s0} ; 2
lsrs.n r2, #1 ; 1
itt cs ; 0 (aligned)
vldmcs.32 r0!, {s0 - s1} ; 1+1+1
vstmcs.32 r1!, {s0 - s1} ; 1+1+1
lsrs.n r2, #1 ; 1
itt cs ; 0 (aligned)
vldmcs.32 r0!, {s0 - s3} ; 1+1+3
vstmcs.32 r1!, {s0 - s3} ; 1+1+3
lsrs.n r2, #1 ; 1
itt cs ; 0 (aligned)
vldmcs.32 r0!, {s0 - s7} ; 1+1+7
vstmcs.32 r1!, {s0 - s7} ; 1+1+7
lsrs.n r2, #1 ; 1
itt cs ; 0 (aligned)
vldmcs.32 r0!, {s0 - s15} ; 1+1+15
vstmcs.32 r1!, {s0 - s15} ; 1+1+15
; Handle the case where we've been asked to transfer <32 words.
; In such a case, count will now be zero, and the Z flag will still
; be set from the last XFER.
;
; Force the branch to use a 32-bit instruction to preserve alignment
; of the loop branch below; this saves a cycle per time that branch
; is taken.
;
; Note that the target of this branch (at 1 below) is also aligned,
; saving a cycle on the rare escape path.
beq.n z1 ; 1 (n.t.)
; All warmed up, transfer in units of 128 bytes.
z0 vldm.32 r0!, {s0 - s31} ; 33
vstm.32 r1!, {s0 - s31} ; 33
subs.n r2, #1 ; 1
bne.n z0 ; ~3 (taken)
; Restore FPU state.
z1 vpop {s16 - s31} ; 17
bx lr ; 1-3??
ENDP ; _Z10copy_wordsPKmPmm
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.