2023-10-20 3:32 PM
Hello,
I'm just started using a nucleo-h742x. I have configured the SPI and the Fatfs library using the default settings, the SPI speed was configured at speed below 1Mbit/s. The sys clock is below 100MHz.
I always get disk_not_ready error when trying to mount the drive (error code 3).
The problem is that I don't see any signal on the MOSI line when a transaction should appear. I have also tried a simple HAL_spi_transmit(), but I have the same problem. I see the clock appearing but no signal on MOSI.
Someone has some suggestions? On other STM32 M4/M3/M0 I have no problem using the same code.
Solved! Go to Solution.
2025-01-26 11:40 PM
How did you solve the problem?
I have the same.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.