2023-10-20 3:32 PM
Hello,
I'm just started using a nucleo-h742x. I have configured the SPI and the Fatfs library using the default settings, the SPI speed was configured at speed below 1Mbit/s. The sys clock is below 100MHz.
I always get disk_not_ready error when trying to mount the drive (error code 3).
The problem is that I don't see any signal on the MOSI line when a transaction should appear. I have also tried a simple HAL_spi_transmit(), but I have the same problem. I see the clock appearing but no signal on MOSI.
Someone has some suggestions? On other STM32 M4/M3/M0 I have no problem using the same code.
Solved! Go to Solution.
2023-10-23 1:32 PM - edited 2023-10-23 1:35 PM
Missing structure members in the example are binary zeros (as normally C static variables and structures are initialized by zeros).
You can find in the SPI include files which symbolic constants correspond to value 0.
Note that in the 1st fragment :
SpiHandle.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
SpiHandle.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_ENABLE;
In the 2nd fragment (generated)
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
2023-10-21 4:04 AM
SPI controller of STMH7 differs from F4, F0 and so on. You can't use *exactly* same code on H7.
Find and study SPI examples in CubeH7 software package, read the RM. Make a simple test or two.
2023-10-21 4:54 AM
H742 has sdio - for sd-card the reasonable interface.
why you dont use it ??
2023-10-21 7:41 AM
In addition I will just remind that all of ST's cache maintenance code is broken:
2023-10-21 10:46 AM
I have looked at the firmware package of H7 but I don’t see a project that can be imported into cubeide with ioc. Any suggestions?
2023-10-21 10:47 AM
I don’t use the sdio because I have SD card module with spi connectivity and I was testing it.
2023-10-22 12:26 PM - edited 2023-10-22 12:29 PM
@frnt The H7 examples have been created before the time point when ST begun including .ioc files with the project. So unfortunately no ready .ioc's there. Suggestions: 1. Try to use the examples as is, without CubeMX or "device configuration tool"; 2. Have somebody produce the .ioc for you.
2023-10-23 12:22 AM - edited 2023-10-23 12:24 AM
I see. I have looked at the SPI example (SPI_FullDuplex_ComPolling), here the initialization of the SPI:
/* Set the SPI parameters */
SpiHandle.Instance = SPIx;
SpiHandle.Init.Mode = SPI_MODE_MASTER;
SpiHandle.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
SpiHandle.Init.Direction = SPI_DIRECTION_2LINES;
SpiHandle.Init.CLKPhase = SPI_PHASE_1EDGE;
SpiHandle.Init.CLKPolarity = SPI_POLARITY_LOW;
SpiHandle.Init.DataSize = SPI_DATASIZE_8BIT;
SpiHandle.Init.FirstBit = SPI_FIRSTBIT_MSB;
SpiHandle.Init.TIMode = SPI_TIMODE_DISABLE;
SpiHandle.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
SpiHandle.Init.CRCPolynomial = 7;
SpiHandle.Init.CRCLength = SPI_CRC_LENGTH_8BIT;
SpiHandle.Init.NSS = SPI_NSS_SOFT;
SpiHandle.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
SpiHandle.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_ENABLE; /* Recommended setting to avoid glitches */
Here is the initialization generated from ioc file:
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 0x0;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi1.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
As you can see, the initialization from .ioc has more parameters than the example.
2023-10-23 1:32 PM - edited 2023-10-23 1:35 PM
Missing structure members in the example are binary zeros (as normally C static variables and structures are initialized by zeros).
You can find in the SPI include files which symbolic constants correspond to value 0.
Note that in the 1st fragment :
SpiHandle.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
SpiHandle.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_ENABLE;
In the 2nd fragment (generated)
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
2023-10-25 11:11 AM
Thanks, the problem has been solved!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.