2026-01-13 2:31 AM
Hello,
I am attempting to measure the current consumption of an STM32L4 before and after entering STOP2 mode using a DC power supply. I expected the initial current of 165mA to drop down to the $\mu A$ range upon entering STOP2 mode, but it only decreased by 5mA.
For my configuration, I have only enabled System Core - SYS - Debug - Serial Wire and a single GPIO pin for toggling to monitor the status via an oscilloscope. When STOP2 mode is activated, I confirmed with the oscilloscope that the GPIO toggling stops completely, indicating the CPU has halted. However, the power supply current remains high.
I have attached my main.c file for reference. Could you please check if I have missed any necessary configurations or if I am doing something wrong?
Thank you in advance for your help.
2026-01-13 5:47 AM
hello @JIN3473
Do you use an ST board or a custom PCB?
The 165mA consumption in normal mode is already very high; it should not exceed a few milliamperes.
If you use a custom PCB, I suspect that there is a short circuit or another issue, especially since your code enters stop mode and you notice a reduction in consumption.
Also, can you specify which STM32L4 product you are using?
to exclude all software related issues, can you try a firmware example and give feedback about the visualized behavior. here is an example using STM32L476RG
BR
Gyessine
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.