2019-06-01 2:54 AM
2019-06-01 3:46 AM
Not yet?
STM32 with cache manage pretty well performance wise with QSPI or OctoSPI external serial memory extension. STM32H series.
2019-06-01 5:13 AM
Might want to ponder the appropriateness of application/task
Several of the L4, F7 and H7 parts support Execute-In-Place via QSPI
Some of the F4/F7 can use SDRAM and NOR, the former could have code packed in NAND
Generally the CM7 parts are recommended as caching is architected into the core
2019-06-01 6:39 AM
The HY-STM32F429IG has NAND and SDRAM, code could be saved into NAND and copied into SDRAM to be run, but execution will be slow, so you'll want to balance where you place critical code.
Rather than in-line screen shots of the web page, just link to it direct;y
https://www.hotmcu.com/hystm32f429ig-development-board-with-independent-lcd-modules-p-263.html
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.