STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 SPI interface to Flash Memory Winbond W25Q80DV

I am trying to interface with the Winbond W25Q80DV which is a SPI flash memory chip. I am using the STM32L476VG development board. To test the connection I am first trying to read the manufacturing ID from the chip. Using an oscilloscope I am able t...

JDarg by Associate II
  • 4184 Views
  • 4 replies
  • 0 kudos

STM32 Beginner: needs help on ADC with STM32F103r8

Hi,I am a beginner for stm32. I am using stm32f103r8 , IAR-ARM IDE.I have attached my celow , this is not working , i am checking it in Proteus 8.8v ( with stm32f103r6). Can anyone help me out with this ?PROGRAM:#include "stm32f10x.h"#include "stm32f...

Pa.6 by Associate
  • 1396 Views
  • 1 replies
  • 0 kudos

File system for spi nand flash

I'm using STM32L496 discovery board and spi nand flash memory..i'm trying to use uffs file system ...is there any porting documentation available for uffs file system into spi nand flash???

aahme.4 by Associate II
  • 1182 Views
  • 1 replies
  • 0 kudos

Can DMA_ADC be used with Memory-to-Memory DMA in fast data acquisition and transfer, as well as noise problem with external PHY?

Hello,I have an application in which waveform is generated (DAC1, updated triggered with T6), data is acquired (ADC1_INP2 and ADC2_INP3, dual simultaneous mode, triggered with T3), T2 is used to control the waveform, ADC_DMA in circular mode is emplo...

QZhao by Associate
  • 890 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.