2023-03-25 12:44 AM
We want to use external 16 bit SDRAM for heap and stack. The SDRAM is configured with byte enable and MPU. I tried to map the memory to 0xC0000000 and 0x60000000, but it doesn't matter. Also the configuration of MPU with MPU_TEX_LEVEL0 or MPU_TEX_LEVEL1 doesn't matter.
An unaligned read/write with 16 bit is possible. So I think a unaligned read/write with 32 bit should possible too, if the compiler handles the access in the right way.
We use GCC 9.3 and it doesn't work.
Here is a code example, which demonstrates the incorrect reuslts.
int i;
uint8_t* pbyte;
uint16_t* pword;
uint32_t* pdword;
uint32_t address;
volatile uint32_t test; address = 0xC0000000;
pbyte = (uint8_t*)address;
for(i=0;i<16;i++)
{
pbyte[i] = i + 1;
}
test = pbyte[0]; // => test = 0x1
test = pbyte[1]; // => test = 0x2
test = pbyte[2]; // => test = 0x3
test = pbyte[3]; // => test = 0x4
pword = (uint16_t*)((int)address);
test = *pword; // => test = 0x0201
pword = (uint16_t*)((int)address + 1);
test = *pword; // => test = 0x0302
pdword = (uint32_t*)((int)address);
test = *pdword; // => test = 0x04030201
pdword = (uint32_t*)((int)address + 1);
test = *pdword; // => test = 0x05040302
pdword = (uint32_t*)((int)address + 2);
test = *pdword; // => test = 0x06050605 instead of 0x06050403
pdword = (uint32_t*)((int)address + 3);
test = *pdword; // => test = 0x07060506 instead of 0x07060504
Is there someone who had the similar problem and has solved it?
2023-04-21 4:37 AM
Did this piece of information come from @Douglas MILLER ?
How does this match the erratum above? I understand that cache fills/evictions may be always aligned, but is there a guarantee for that by the cache/processor?
JW
2023-04-21 5:12 AM
TBH this does not make much sense to me.
In post March 27, 2023 you set the FMC area as Normal Cached Write-back, and you've said it does not work. Write-back caching would imply that only writes to FMC are from cache evictions, which are presumably always properly aligned (Cortex-M7 TRM, 5.4.7 AXIM interface transfers, Cache line write-back (eviction))
Now you say, that you set it as Normal Cached Write-through, and it works? Write-through writes IMO could end up at the FMC interface as unaligned (Non-cacheable, Write-Back no Write-Allocate or Write-Through writes subchapter of the same chapter, Table 5-17 STR to Cacheable write-through or Non-cacheable Normal memory).
I am confused and feeling quite lucky I don't have to deal with the 'H7.
JW
2023-04-21 12:38 PM
> feeling quite lucky I don't have to deal with the 'H7.
Yep. Some STM32H7 have erratum that says that Write-through is NOT recommended, instead use Write-back. But here the OP says that write-through does work...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.