2025-07-16 12:41 AM
Hello friends : )
I've recently tested the NUCLEO-G491RE board for an upcoming redesign.
Current design relies on quite tough interrupt latency so here is where I begun.
As I understand, with no FPU usage (in isr) (ASPEN + LSPEN = 0) one could expect up to 12 SYSCLK latency.
In this case 75ns at 160MHz which sounds pretty decent (today it's about 73ns).
I started off by creating two very similar interrupt services I intended to toggle between.
Each would pulse a output pin and trigger the other one:
Attributes: 'interrupt' + optimize("-O2")' + 'section(".RamFunc")' + 'aligned(8)' + 'naked'
static void onTimeStampEvent(void)
{
GPIOA->BSRR = 1<<12;
NVIC->ISPR[1] = 1<<(39-1*32); // USART3
GPIOA->BRR = 1<<12;
#ifdef NAKED
__ASM volatile ("BX LR":::);
#endif
return;
}static void onReceiveEvent(void)
{
GPIOB->BSRR = 1<<14;
NVIC->ISPR[0] = 1<<(11-0*32); // DMA1_CH1
GPIOB->BRR = 1<<14;
#ifdef NAKED
__ASM volatile ("BX LR":::);
#endif
return;
}In main the usual suspects:
Finally, the main loop:
u = 0;
while(1)
{
NVIC->ISPR[0] = 1<<(11-0*32); // DMA1_CH1
u++;
}
This works splendidly, sort of...
<PicoScope shot 1>
The total time for a complete round trip is about 381ns or 61 SYSCLK.
Variable "u" in main never changes from "0" suggesting expected continuous interrupts.
The thing is, would not tail-chaining occur?
Now I tried diversify priority levels, yellow being less important:
<PicoScope shot 2>
Priority in action, indeed, however now a round trip takes 562ns (90 SYSCLK).
Still no tail-chaining, and worse, lots of extra time for the same amount of work.
Where have I done wrong?
Any help appreciated = )
/Hen
2025-08-06 11:52 PM
I don't quite understand what you are trying to say here, but as I've said above, the best strategy with Cortex-Mx (and modern 32-bitters in general), when it comes to hard real-time operation, is to strive to use purely hardware as much as possible. Factors which potentially impact interrupt latencies and jitter are just too many, and they tend to be poorly documented.
JW
2025-08-09 10:15 PM
Yes, I agree on that point, relying on instruction feed with real time requirements is problematic.
In our case the DMA takes the hard part, but the result has to be analyzed and ready before the next event.
The 30ns spread is what the DMA usage offers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.