2017-11-23 4:15 AM
Hi.,
I am working on STM32F767ZI Nucleo board, In this I am trying to interface external audio board through I2S interface, I configured I2S in Master receive mode using STM cubeMX, But I am not able to receive any data. I also cross checked signals on board , I2S_A_CK clock is coming (48K), but I2S_WS & I2S_SD(data) signals are not coming . Can you please tell me what could be the issue .
I2S configurations:
hi2s2.Instance = SPI2;
hi2s2.Init.Mode = I2S_MODE_MASTER_RX; hi2s2.Init.Standard = I2S_STANDARD_PHILIPS; hi2s2.Init.DataFormat = I2S_DATAFORMAT_24B; hi2s2.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE; hi2s2.Init.AudioFreq = I2S_AUDIOFREQ_48K; hi2s2.Init.CPOL = I2S_CPOL_LOW; hi2s2.Init.ClockSource = I2S_CLOCK_PLL;Receive function I am using :
HAL_I2S_Receive_IT(&hi2s2, I2S_Buffer_Rx, 100);
I hope I2S_CK & I2S_WS signal must generate , without these two signal audio board doesn't send any data. Can you please suggest if any changes required in above initialization.
Thank you
#nucleo-board #i2s #stm32-f7We’re moving the ST Community to a new platform to give you a better and more reliable community experience.