2017-09-06 11:07 PM
could it be that in STM32Cube_FW_F4_V1.16.0\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_IAP
the latest firefox is not supported?
FW download via internet explorer works but but not firefox 55.0.3 (32-Bit) !
Thx
2017-11-22 1:10 AM
HAJJEM.Oussema
Can you comment on this issue?
The ST is code in this project is meant to work with firefow as well. But it doesnt!
Same applies to google chrome browser
Is ST going to fix this?
2017-11-23 2:58 AM
Hello,
I confirm that some regressions are available when using last Firefox versions, this will be reported to be fixed in the next STM32CubeFW F4 releases.
Thanks and regards,
Oussema.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.